This is the first series of events that will be done by the Brilon transformer plant. At each location, around 15 customers are expected to attend from different industry segments like pulp and paper, chemical industry, utilities etc.
Through this nationwide tour the guests will receive helpful and interesting information about the RESIBLOC and EcoDry transformer technology. In addition, the TriDry transformer - the ABB innovation in the field of dry-type transformers - will find special attention. Besides the speeches of our ABB experts, one customer in the region will present his experience with the ABB transformer. According to the motto of the tour "Experiencing transformer technology firsthand", all participants will also have detailed insights into the structure and functioning of our technology with the EcoDry and TriDry exhibition units.
The tour is fully advertised within the current ABB media, including the official ABB German website and in the German customer magazine "Connect". In addition, the roadshow will be communicated in selected specialized online portals via online banners.
For more information please visit www.abb.com/resibloc-tour or contact Anne Heeke, anne.heeke@de.abb.com