The System pro E® energy range provides commercial and industrial end-users with easy to install, flexible and safe applications that can integrate all types electrical devices to build distribution panels up to 800A. It is the first ABB solution that combines ABB technology and the former GE Quixtra platform to provide a ‘best of both’ technology solution.
Installing the System pro E® energy range can have a significant positive impact on overall efficiency for the end-user, with ABB estimating it can save up to 40 percent in assembly time. It also requires 30 percent less stock, 15 percent fewer order codes and improves wiring space capacity by 20 percent. This increase in operational efficiency can also help optimize energy distribution– a key feature of ABB’s smart energy management technologies.
The System pro E® range consists of wall-mounted and floor-standing sheet steel cabinets, as well as busbars and functional units, and allows maximum flexibility for the panel builder and installer to build distribution boards for any application.
The range is also extremely safe - the System pro E® energy L provides a protection degree up to IP43 and the System pro E® energy M, the mono-block solution - up to IP55. When combined with ABB’s DIN-Rail devices the range is also certified to IEC 61439 standard.
In addition, System pro E® energy Combi facilitates internal configuration with a modular system that includes all the individual parts required for assembly. This allows the end-user to take a flexible approach towards stock keeping and avoid a time-consuming search for system parts, such as brackets, screws or fasteners.
Piero-Giorgio Schiannini, Global Product Group Manager Energy Distribution, comments: “ABB is always striving to develop solutions that allow customers to save time and money, through a combination clever design and smart technology. Our new System pro E® energy range of sub distribution boards combine with connectivity devices to provide effective digital energy management solutions for commercial and industrial applications. The technology is flexible, easy to assemble and meets the highest safety standards. This means that installers and end-users can be confident that they are using the most safe, reliable and efficient solution for their energy distribution.”

ABB (ABBN: SIX Swiss Ex) is a technology leader that is driving the digital transformation of industries. With a history of innovation spanning more than 130 years, ABB has four, customer-focused, globally leading businesses: Electrification, Industrial Automation, Motion, and Robotics & Discrete Automation, supported by the ABB Ability™ digital platform. ABB’s Power Grids business will be divested to Hitachi in 2020. ABB operates in more than 100 countries with about 144,000 employees. www.abb.com
ABB’s Electrification business is a global leader in electrical solutions, operating in more than 100 countries, with over 200 manufacturing sites. Approximately 53,000 employees are dedicated to delivering the future of safe, smart and sustainable electrification, for industries, public services and communities. With advanced ABB AbilityTM enabled digital solutions at its core, our portfolio protects, connects and optimizes electrical energy supply. This includes the powering of industry, infrastructure and transportation, from data centers to smart buildings and e-mobility solutions; the integration of renewables; and the delivery of intelligent distribution and energy storage. For more information visit https://go.abb/electrification