ABB Ability™ Digital Powertrains monitoring services provide advanced analytics and maintenance planning to ensure the efficient operation of powertrain equipment, including drives, motors, bearings and pumps.
A suite of digital solutions including devices, software and services is the centrepiece of ABB’s stand, PC41, at the International Quarrying and Recycling show, Hillhead Quarry, Buxton, UK, 26-28 June 2018.
ABB Ability Digital Powertrains monitoring services enable users to digitally “see” operational variables through an integrated, one-stop portal.
The first integrated service in the industry is ABB Ability™ Condition Monitoring for powertrains – for drives, motors, bearings and pumps. This visualises key operational parameters of individual assets as a unified system and, with the help of ABB’s expertise, provides customers insight into maintenance to ensure optimal operations. As a result, ABB Ability Condition Monitoring for powertrains offers insight that leads to operational improvement, resulting in less downtime, extended equipment lifetime, lower costs, and higher profitability.
The service offers full transparency on all parameters of powertrains usage, generating notifications when detecting indicators, such as temperature variations, unusual vibrations and fault notifications. Customers can receive a thorough report on equipment status and further maintenance recommendations.
ABB Ability™ Condition Monitoring for motors:
This solution includes a smart sensor device attached to a low voltage motor to remotely monitor the motor via an app or web portal. The service enables predictive analytics that can boost uptime while reducing energy consumption.
ABB Ability ™ Condition Monitoring for drives:
This service offers real-time information about connected drives events. Monitoring parameters include drives availability, environmental conditions and fault events. The service offering helps anticipate possible operational issues and maintenance needs.
ABB Ability™ Smart Sensor for pumps:
This collaboration between ABB and Swiss pump manufacturer, Egger Pumps, includes a smart sensor for pumps, focusing on wastewater plants. This solution was jointly developed to monitor pump temperature, vibration and bearing condition – using data analytics – to prevent clogging and other issues in the application.
ABB Ability™ Smart Sensor for mounted bearings:
This solution connects to ABB’s Dodge® mounted bearings to give a health indication on this asset in the powertrain. Bearings are a critical component in the overall system and can be an initial indicator of problems in the powertrain.
ABB Ability™ Predictive Maintenance for drives:
This service combines data, machine learning and ABB’s expertise to regularly monitor and analyze data in the cloud to deliver actionable insight and improvements for installed high demand drives.
Reference information:
Digital Powertrains: an intelligent powertrain, equipped with sensors and cloud connectivity, comprises motors/generators, drives/converters, mechanical powertrain components including bearings, couplings and gearboxes, and an application such as a pump.
ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner of Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 135,000 employees. www.abb.com