The new ‘continuous evaluation’ function allows the software to use engine data gathered by edge computing services, adding a new dimension to Tekomar XPERT’s monitoring, reporting and advisory capabilities.
“Continuous evaluation allows for the cloud-to-cloud transfer of engine data from edge computing platforms to Tekomar XPERT,” said Pascal Reolon, Product Manager, ABB Turbocharging. “The result will be faster access to more engine data from which to draw even quicker insights to optimize engine performance.”
Combined with Tekomar XPERT’s already wide compatibility with other data systems (such as fleet performance software), the function enables ABB to offer remote continuous performance evaluation, with instant comparison of an engine’s current performance with its digital twin, from which Tekomar XPERT draws advice for optimizing performance. Automating the data gathering process for performance evaluations will ensure greater accuracy and more frequent reporting, as well as reducing crew workload.
Edge computing allows large volumes of data to be processed before being transferred to the cloud for storage. It is ideal for environments that may not always have a guaranteed internet connection, such as ships. Continuous evaluation can be used to collate data from any platform that sends data to the cloud. Vessels will need to install any data collection and transmission hardware required by the edge computing platform provider as well as subscribing to Tekomar XPERT.
The function is another step in the development of the Tekomar XPERT product family, with regular six-monthly releases providing subscribers with additional connectivity and diagnostic features. Tekomar XPERT runs on any engine, regardless of type or age. It is built on ABB’s Ability™ platform with the highest standards of cyber security.
ABB Turbocharging (www.abb.com/turbocharging) is at the helm of the global industry in the manufacture and maintenance of turbochargers for 500 kW to 80+ MW diesel and gas engines. Our innovative leading-edge technology enables our customers to increase their performance; producing lower emissions, and improving fuel consumption even in the toughest environments. Approximately 200,000 ABB turbochargers are in operation across the globe on ships, power stations, gen-sets, diesel locomotives and large, off-highway vehicles. We have over 100 Service Stations in more than 50 countries globally and a wide service portfolio that guarantees Original Parts and Original Service anytime, anywhere.
ABB (ABBN: SIX Swiss Ex) is a technology leader that is driving the digital transformation of industries. With a history of innovation spanning more than 130 years, ABB has four customer-focused, globally leading businesses: Electrification, Industrial Automation, Motion, and Robotics & Discrete Automation, supported by the ABB Ability™ digital platform. ABB’s Power Grids business will be divested to Hitachi in 2020. ABB operates in more than 100 countries with about 144,000 employees. www.abb.com
For more information please contact:
Media Relations ABB Switzerland Ltd, Turbocharging
Mei Lee Bruggerstrasse 71a
Senior Global Media Relations Manager 5401 Baden, Aargau, SWITZERLAND
Mobile: +41 (0) 79 627 6388
Phone: +41 58 58 51874