The success story of ABB’s childcare centers began 50 years ago. They were modern then and are still modern now.
The best for children and their parents
It was no less than half a century ago that the company then known as BBC opened Switzerland’s very first child day nursery. The company was fulfilling its social responsibility towards guest workers from Italy and Swiss society: a piece of active integration. ABB built heavily on this idea. Professional, caring, facilitative care is now a major factor in attracting people to work at ABB, which is constantly on the lookout for highly qualified employees. It is also a flexible answer to the multiple challenges presented by a society that needs to accommodate working parents.