Keeping operations moving during a critical upgrade

Keeping operations moving during a critical upgrade

With more than 1,000 significant commercial developments choosing Stanilite’s emergency lighting solutions in the last 10 years, a stand-out example of the Platinum range’s triple-win value is Westfield Helensvale in Queensland.

With more than 1,000 significant commercial developments choosing Stanilite’s emergency lighting solutions in the last 10 years, a stand-out example of the Platinum range’s triple-win value is Westfield Helensvale in Queensland.

Launching in 2005, the centre’s original emergency lighting system had become expensive to maintain, with high energy consumption. The ABB team was set the challenge of offering an alternative solution to improve performance and reliability, and reduce costs – all while ensuring minimal impact to the centre’s operations.

Stanilite’s Nexus RF backbone was installed in key locations and its wireless set-up meant that each fitting could be replaced and commissioned without the need for additional cable.

The ability to retrofit the facility to Stanilite’s Nexus solution was just the start of time and cost savings. Staged delivery over a four-year period has ensured no impact to operations, and the facility manager now has immediate access to detailed performance reports, driving even greater safety performance through real-time visibility of the entire emergency lighting network.

With the ABB team offering 45 years of engineering history, alongside manufacturing excellence that ensures complete compliance with AS/NZS 2293 standards, the short and long-run benefits of its Stanilite emergency lighting are unmatched. Continual R&D improvement and the team’s constant eye on lifetime value drive even greater safety assurance, backed by a competitive cost proposition.

Links

Contact us

Downloads

Share this article

Facebook LinkedIn Twitter WhatsApp