ABB’s UniPack-G provides safety and reliability for Argentina’s largest electricity distribution company

ABB’s UniPack-G provides safety and reliability for Argentina’s largest electricity distribution company

ABB provides innovative solution with the UniPack-G Compact Secondary Substation.

Edenor S.A., the largest electricity distribution company in Argentina, has selected ABB to help meet the country’s energy distribution challenges.

Headquartered in Buenos Aires, Edenor S.A. distributes power to approximately 20 percent of the country. With the region facing challenges ranging from increasing energy demands to declining reserve margins, Edenor was looking for a partner to provide its customers with a smart, safe, and efficient distribution solution.

ABB’s experts explained the benefits of using the UniPack-G CSS (Compact Secondary Substation), including high safety and reliability, along with ease of maintenance and installation. Ultimately, the customer chose to use the UniPack-G with its GRP (glass reinforced polyester) enclosure to aid the distribution of auxiliary energy to high- and medium-voltage substations.

By using ABB’s patented GRP material for the enclosure in the UniPack-G CSS, all of the equipment within was protected by a housing that has the strength and durability of concrete with the lightweight characteristics of steel. Its internal components have a prolonged lifespan, due to the strong thermal characteristics of the UniPack-G enclosure. Additionally, it was lightweight enough to be easily transported.

The IEC 62271-202 classified solution also introduced high-end thermal and mechanical properties while assuring safety for personnel and the general public in the event of an internal arc.

“This type of housing provides significant flexibility for internal compartmentation,” a project engineer from Edenor S.A. explained, “along with a new concept for small substations and the security of a type tested solution.”

“We are delighted to partner with Edenor S.A. and look forward to a continued relationship as we write the future of safe and sustainable energy distribution in Argentina,” said Alessandro Palin, President of ABB’s Distribution Solutions Division.

The UniPack-G is installed in part of the Federal Capital and Buenos Aires surroundings and furthermore could be used on future projects. It is equipped with UniSec air-insulated secondary switchgear.

ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 110,000 talented employees in over 100 countries. www.abb.com

ABB’s Electrification Business Area is a global leader in electrical products and solutions, operating in more than 100 countries, with over 200 manufacturing sites. Our 50,000+ employees are dedicated to delivering safe, smart and sustainable electrification. With ABB AbilityTM enabled digital solutions at its core, our portfolio protects, connects and optimizes the flow of electrical energy for smarter electricity distributionfor utilities, industry, buildings, infrastructure and mobility. For more information visit https://go.abb/electrification

Links

Contact us

Downloads

Share this article

Facebook LinkedIn Twitter WhatsApp