ABB delivers sustainable shore connection technology for Viking Line’s high-speed ferry

ABB delivers sustainable shore connection technology for Viking Line’s high-speed ferry

ABB Marine & Ports latest shore connection technology is ensuring that calls by the passenger ferry Viking XPRS at Estonia’s Port of Tallinn are made quietly, efficiently and emissions-free

The well-known ferry, built in 2008, is deployed on the 2.5-hour route across the Baltic Sea between Tallinn, Estonia, and Helsinki, Finland, typically docking in the Estonian city twice a day.

Shore connection technology from ABB is designed for easy integration on all ship types and is controlled from the vessel itself, so that sequencing does not need intervention by any shore-based staff. Its sustainable in-harbor operation is especially valued at city ports such as Tallinn, which can have a significant impact on local air quality. Given the frequency of port calls made by Viking XPRS, shore connection will also save substantial amounts of fuel.

Earlier this year, Port of Tallinn installed the latest ABB shore power systems on five of its piers in Old City Harbour as part of the first shore power project in Estonia, enabling vessels with shore power technology to draw on land-based power in port.

ABB Shore Connection for Viking XPRS
ABB Shore Connection for Viking XPRS
center

“ABB’s shore connection is the latest initiative in our ongoing sustainability program,” said Johanna Boijer-Svahnström, Senior Vice President, Corporate Communications, Viking Line. “Installing the shore connection system on board Viking XPRS, and having the shore power available in the Port of Tallinn will make a significant contribution to clean air within the port and its surroundings. We have successfully collaborated with ABB on a number of projects, and the fact that ABB provides installations aboard ship and in port, with prompt delivery and backed up by 24-hour support, has proved compelling.”

“It is an honor to support Viking Line in its journey toward sustainable shipping,” said Jyri Jusslin, SVP and Head of Service at ABB Marine & Ports. “Our shore connection is designed for all types of ships, with safety and simplicity in mind. This is also another key step in ensuring that Baltic Sea ports continue on their forward-looking path to eliminate emissions.”

ABB’s full scope of supply for Viking XPRS included a shore connection control board with three separate ship-shore communication links, ensuring fail-safe connections at all times. ABB has also provided the medium-voltage switchgear, an 11kV-400V transformer, a circuit breaker bypass arrangement for drydock connection, and a low-voltage main switchboard breaker. The delivery meets the new IEC-standard for shore connections, which demand higher levels of safety and environmental performance than ever before at the shipside. Commissioning was executed during the vessel’s normal operation.

As a leader in electric shipping and smart port technology, ABB Marine & Ports offers comprehensive shore connection solutions comprising state-of-the-art infrastructure both onshore and on board ship. Systems are compliant with international regulations and include high- and medium-voltage switchgears, transformers, frequency converters, control and protection systems, and more.

ABB Marine & Ports supplies world-leading technologies that are driving the evolution of sustainable shipping. Electrical propulsion, data-driven decision support and integrated solutions for ship and shore from ABB are paving the way to a zero-emission marine industry, providing greater efficiency and reliability to shipowners, and preparing vessels to meet the demands of tomorrow. Our automation and electrical solutions are making port and terminal operations safer, greener and more productive. ABB Marine & Ports operates in 26 countries and has 2,000 employees. www.abb.com/marine

ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 110,000 talented employees in over 100 countries. www.abb.com

Contact us

Share this article

Facebook LinkedIn X WhatsApp