German media publisher secures ABB expertise for press management and optimization system upgrade

Rheinisch-Bergische Druckerei GmbH, which prints well-known newspaper Rheinische Post, will use ABB’s MPS Production systems and software to optimize printing processes and reduce costs and maintenance

Global technology company ABB has been awarded a contract to provide software system upgrades including its MPS Production and production data analysis system MPS Inform to Rheinisch-Bergische Druckerei GmbH.

Based in Dusseldorf, the company publishes daily, weekly and monthly newspapers, periodicals and magazines for customers in Germany. These include the Rheinische Post, Westdeutsche Zeitung, Rem­scheider Generalanzeiger and the Solinger Tageblatt. These are produced in a print run of around 600,000 copies along with 3.3 million advertising papers and magazines. The Rheinische Post has the largest circulation of all the daily newspapers in the Rhineland region with more than 268,800 copies reaching about 740,000 readers daily.

MPS Production is an ABB press management and optimization system, which enables operators to plan print products using specifications imported from an external system or created using an inbuilt graphical planner. The tooling package also maps out printing presses installed on site for complete end to end production optimization using currently available infrastructure.

ABB's printing optimization package will help reduce costs and maintenance
ABB's printing optimization package will help reduce costs and maintenance
center

Rheinisch-Bergische Druckerei GmbH will also achieve reductions in preparation time, start-up waste and ink and water use, bringing significant cost savings, through MPS Systems.

“We’re looking forward to benefitting from ABB’s decades of industry experience, systems knowledge and service, bolstered by learnings gained from a diverse range of production optimization applications globally, said Kirsten Klaszus, Managing Director at Rheinisch-Bergische Druckerei GmbH. “These latest upgrades will ensure that we are fit for the future of an industry that continues to work to tight financial margins.”

The ABB tools will assist operators and create virtualization of the system though conversion to run with PostgreSQL, allowing independence from the hardware and operating system lifecycle. This enables the application to be tested on and moved to a new platform when required, increasing availability and backup solutions.

“Our technologies have developed beyond recognition since we first worked with Rheinisch-Bergische Druckerei GmbH more than 35 years ago,” said Damian Staedeli, Head of Printing, ABB. “We are looking forward to seeing our customer realize the benefits of working with such a flexible system that provides oversight of the whole printing process and ease of operation.”

The software system upgrades will be delivered to Rheinisch-Bergische Druckerei GmbH and will replace obselete hardware operating systems in early 2021.

ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 110,000 talented employees in over 100 countries. www.abb.com

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp