ABB India launches a new range of circuit breakers for electrical retail market

The complete Formula DIN range of circuit breakers are designed and developed under the ‘Make In India’ program for all types of residential and commercial buildings.

ABB India has launched Formula DIN-Rail, a complete range of Miniature Circuit Breakers (MCBs), ResidualCurrent Circuit Breakers (RCCBs) and Isolators for the electrical retail market which is estimated to beworth 250 million USD in India.

The ABB Formula DIN-Rail portfolio with its contemporary design, provides optimum protection toelectrical circuits from possible damages caused by overload, short circuits, and earth leakages inbuildings. The MCBs are available with a seven year warranty, which is a first in the Indian electrical market.This range meets international standards and is manufactured in ABB’s Smart Buildings factory located inBengaluru, with a production capacity of 12 million pole of MCBs per year.

ABB Smart Buildings launch Formula DIN Rail video
“Our range of protection devices is designed to significantly improve electrical performance of bothresidential and commercial units, creating safe, sustainable homes and buildings for the future,” said CPVyas, President- Electrification business, ABB India Ltd.

The entire range of MCBs, RCCBs and Isolators are available through the ABB Electrification business retailnetwork across India as well as on ABB eMart, the company’s online marketplace. The portfolio comes witha lowest watt loss and space for better air circulation, as well as clear ON/OFF indications printed on allthe products for ease of use.

The ABB Formula DIN-Rail portfolio is a sophisticated piece of engineering that also enables a fit withdifferent pole configurations, includes B/C tripping characteristics (MCBs), various leakage sensitivity(RCCBs) and Isolation (Isolators) up to 63 A for residential and similar applications.

The SW200 M MCBs, which are part of this range, perform the most crucial tasks of preventing an overloadon the electrical circuit by tripping before the cable is damaged. These MCBs not only satisfy the mostcommon MCB requirements but can also be installed in any residential or similar environment, makingthem flexible and reliable for the end user. This ISI approved range provides complete protection from 6-63Ampere in B & C Curve with 7 years of warranty and standardized IEC60898 International and IS 60898-1Indian certification.

Formula DIN Rail Product video

The FW200 RCCBs in this range ensure safety of people and installations from earth leakage current, in asystematic and calculated way. This ISI approved device works on continuous calculations of the systemline currents to detect the flow of current to earth, thereby preventing accidental electric shock by direct orindirect contact, as well as protecting installations against the risk of fire. It is also approved byinternational standards IEC 61008-1 and IS 12640-1(2016).

Furthermore, the SDW200 Isolators, which are part of the ABB SW range, provide state-of-the-art safetyand comfort by separating a part of the system for conducting secure maintenance activity and is also ISIapproved.

ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation ofsociety and industry to achieve a more productive, sustainable future. By connecting software to itselectrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology todrive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’ssuccess is driven by about 110,000 talented employees in over 100 countries. www.abb.com

ABB’s Electrification Business Area is a global leader in electrical products and solutions, operating inmore than 100 countries, with over 200 manufacturing sites. Our 55,000+ employees are dedicated todelivering safe, smart and sustainable electrification. With ABB Ability™ enabled digital solutions at itscore, our portfolio protects, connects and optimizes the flow of electrical energy, including the integrationof renewables and energy storage for smarter electricity distribution for utilities, industry, infrastructureand transportation. For more information visit https://go.abb/electrification

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp