ABB expands Dodge® Passport selection tool with belt conveyor design program

Passport, an online product selection program, now offers users an application-based approach to quickly and easily design and order mechanical products used in belt conveying applications

Passport is responsive in design for use across many devices.
Passport is responsive in design for use across many devices.
center

ABB enables customers to design conveyor pulley assemblies and belt conveyors for the first time with its web-based Dodge Passport design tool. These user-friendly programs allow customers to create and order complete application-based solutions for bulk material handling applications typically found in mining, cement, aggregate and grain industries. 

Passport’s new conveyor pulley assembly designer allows users to select, quote and order conveyor pulley assemblies complete with shafting and mounted bearings. Real-time pricing and availability enables customers to make cost-effective selections of readily available components. After selections are complete, Passport offers add-to-order capability, allowing customers to seamlessly convert selections into orders via the PT Place e-commerce platform.

For the new belt conveyor design program, Passport uses application-specific design parameters such as capacity, material characteristics, and conveyor geometry to accurately size gear reducers, motors, conveyor pulleys, shafting, and mounted bearings.  Passport also delivers a comprehensive summary that includes component details, supporting technical performance data and indexes selections for future reference.

“From Torque-Arm reducer drive packages to conveyor pulley assemblies complete with mounted bearings, Dodge has a leading product offering for belt conveying applications,” says Matthew Wolford, Electronic Tools Product Manager.  “Passport’s new design applications leverage over 140 years of bulk material handling expertise, guiding users through a reliable selection process for all Dodge mechanical products and accessories.”

Future Passport capabilities will incorporate additional Dodge mechanical power transmission products, as well as expanding the application-based approach for packaged product solutions to a wider range of common industrial applications.

 For more information please visit dodgepassport.abb.com

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in power grids, electrification products, industrial automation and robotics and motion, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner in ABB Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 147,000 employees. www.abb.com

Contact us

Share this article

Facebook LinkedIn X WhatsApp