ABB’s new ReliaGear™ LV MCC is the next level in motor control centers

Combining decades of GE Industrial Solutions motor control center (MCC) experience with ABB’s cutting-edge, digital technology in both the ACS580 variable frequency drives and Tmax® XT circuit breakers, ReliaGear™ LV MCC offers the best of both worlds.

ABB today announced the release of ReliaGear™ LV MCC. The low voltage motor control center is built for simplicity and durability. Designed for safety, this low-voltage MCC was created to meet customer needs across a wide range of applications with a focus on smart MCC solutions. ReliaGear LV MCC is UL/cUL 845 listed and available globally in all ANSI markets where NEMA standards are prevalent and/or required.

“Customer feedback started ABB on the journey to build a simple, smart MCC with a wide variety of features and functionality,” said Dick Jackman, Global Product Group Manager for ANSI MV+LV Switchgear, ABB. “The result, ReliaGear LV MCC, brings more advanced protection and controls to the ABB portfolio, enhancing both quality and reliability.”

ReliaGear LV MCC is engineered for use in demanding applications in market segments such as pulp and paper, mining and metals, utility, chemical, oil and gas, mass-production manufacturing, and water and wastewater. The ReliaGear LV MCC motor control center provides a safer, smarter, and more sustainable solution to protect and control motors.

ReliaGear™ LV MCC
ReliaGear™ LV MCC
center

Safer: Retractable stab mechanism allows for closed-door racking, helping keep operators safe from potential arc flash hazards. Integrated surge protection device mitigates risk from surge events, such as lightning, which can cause equipment failure and downtime. Reinforced door latches are 21x stronger than previous designs.

Smarter: ACS580 variable frequency drives are compatible with a wide range of fieldbus protocols meaning the drives, breakers, relays, etc. speak many communication protocol "languages" allowing for easy integration with other systems, including non-ABB systems. Wide range of motor management relays, including ABB's UMC100.3, allows for communication, protection and control. Tmax XT molded case circuit breakers offer the option for Ekip trip units with added ability for digital protection, management, measurement and remote monitoring.

Sustainable: Robust design and strong assembly allow for an IBC-2018 and CBC-2019 seismic rating. Plug starters up to Size 5, allow easy installation and removal. Newly designed disconnect handle is more robust, increasing durability during the life of the MCC.

For more information on features and benefits of ReliaGear LV MCC, please see https://electrification.us.abb.com/products/motor-control-centers/reliagear-lv-mcc.

ABB (NYSE: ABB) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 105,000 talented employees in over 100 countries. www.abb.com

ABB’s Electrification BusinessArea is a global leader in electrical products and solutions, operating in more than 100 countries, with over 200 manufacturing sites. Our 50,000+ employees are dedicated to delivering safe, smart and sustainable electrification. With ABB AbilityTM enabled digital solutions at its core, our portfolio protects, connects and optimizes the flow of electrical energy for smarter electricity distributionfor utilities, industry, buildings, infrastructure and mobility. For more information visit https://go.abb/electrification

—
For more information please contact:

Media Relations


Melissa London

Phone: +1 919 649 6581
Email: melissa.london@us.abb.com

—

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp