Power over Ethernet (PoE) offers several benefits for process engineers, as it omits the need for a separate DC power infrastructure, providing power and communications via the same cable. This brings new agility as flowmeters can be installed wherever needed. In addition, ABB 4-wire Ethernet combines classic outputs with future communication protocols. Offering a modular design allows the combination of both worlds and ensures that devices are future-proof, increasing the longevity of the flowmeters.
Furthermore, flowmeters with Ethernet connectivity increase simplicity, flexibility and reliability to operations in process automation, while enhancing real-time visibility of data. Previously hidden data in field devices, such as measurement values on density, conductivity or concentration of the medium, can be unlocked. This in turn will help customers across all industries identify redundant measurement points in their plants to achieve savings along the way.
Frank Frenzel, Global Product Line Manager Process Flowmeters, shares “ProcessMaster and CoriolisMaster with Ethernet will support our customers’ digital journey towards smart cities and Industry 4.0. Ethernet is the leading communications technology. By incorporating it into the ABB flowmeters, we can help even more customers reduce complexity of operations and lower costs of infrastructure in more plants around the world – safely and remotely.”
An integrated secure web server based on the ABB Ability™ Cyber Security framework ensures robust and secure operations that offer instrumentation engineers support during commissioning and troubleshooting. It also provides access to configuration, diagnostics and measurement data through a built-in QR code. This allows verification of all parts of the flowmeter and provides insights into its operating condition with automatically generated reports.
Combining 4..20 mA or digital outputs with new 1- or 2-port Ethernet makes classic instrumentation truly future-proof, with speeds of up to 100Mbit/s. The flowmeters use various Ethernet based communication protocols, such as simple Modbus TCP or high performance EtherNet/IP. This prepares them for IT/OT convergence, cloud connectivity and the requirements needed for secure and encrypted communication both today and tomorrow.
*Ethernet connectivity for the electromagnetic flowmeter ProcessMaster is currently available in North America only. It will be released globally later in 2021.
ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 105,000 talented employees in over 100 countries. www.abb.com