ABB has launched ABB Ability™ Condition Monitoring for belts, an advanced digital service to enable mine operators to track speed, misalignment, damage, thickness and wear, slippage and temperature of conveyor belts in real time, and therefore anticipate maintenance, avoid unplanned downtime and improve belt reliability and lifetime.
Belt damage can cause significant production time loss in mines and processing plants with in-person inspections typically carried out to determine the condition of conveyor belts. The new ABB Ability™ Condition Monitoring for belts offers a complete overview of the assets’ condition through continuous monitoring of belt health, generating alarms and warnings in the event of deterioration. By moving from preventative to predictive maintenance, it enables operators to avoid the costly failures that can occur between physical inspections and personnel can be removed from dangerous areas.
“Australian mines operate in some of the most remote and harshest environments in the world, so it is critical to anticipate maintenance and avoid unplanned downtime,” said Stuart Cowie, Head of Process Industries, ABB Australia. “Through our unique digital expertise, the ABB Ability Condition Monitoring for belts solution enables mine operators to track speed, misalignment, damage and wear to conveyor belts in real time and improve belt reliability and lifetime of their equipment.”

The technology is based on sensors installed in strategic points of the conveyor belt equipment and is specifically designed to withstand harsh environments while monitoring asset health and condition.
ABB Ability™ Condition Monitoring for belts provides easy access to informative dashboards. Fault trend analysis, event alarms, data logs and reports can be monitored for single or multiple conveyors and by remote connection, SMS text message and email.
“Real time monitoring of the actual belt performance prompts the necessary corrective actions ahead of failure or further and more costly damage,” said Eduardo Botelho, Global Material Handling Service Product Manager, ABB. “With equipment condition continuously assessed, operators can plan necessary maintenance only when certain indicators give the signal that the equipment is deteriorating, and the probability of failure is increasing. It will consistently catch misalignment or speed issues online, long before failure, and pre-empt issues such as falling material, energy waste, excessive belt wear, rupture or fire.”
The solution can work as a stand-alone option or can be integrated into any control system, being interoperable with existing maintenance tools and infrastructure. KPIs can be customised, based on customer's needs or pain points.
—
ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energises the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 105,000 talented employees in over 100 countries.
Process Automation: ABB’s Process Automation business is a leader in automation, electrification and digitalization for the process and hybrid industries. We serve our customers with a broad portfolio of products, systems, and end-to-end solutions, including our #1 distributed control system, software, and lifecycle services, industry-specific products as well as measurement and analytics, marine and turbocharging offerings. As the global #2 in the market, we build on our deep domain expertise, diverse team and global footprint, and are dedicated to helping our customers increase competitiveness, improve their return on investment and run safe, smart, and sustainable operations.
|