ABB helps Pulse Fitness & Spa customers charge while they train

ABB helps Pulse Fitness & Spa customers charge while they train

  • ABB to deliver electric vehicle chargers to Pulse Fitness & Spa locations in Sofia, Plovdiv and Bankso
  • Terra 124 DC chargers can charge two EVs simultaneosly

ABB delivered 7 Terra 124 DC charging stations to the well-known sports center chain Pulse Fitness & Spa at its locations. The charging stations - owned, installed and operated by ABB’s partner Fines Charging - can charge electric vehicles with 120 kW power, depending on the electric vehicle and the number of EVs charged at the same time.

This new addition to Pulse Fitness & Spa’s range of offered services will provide its customers with the comfort of being able to charge their electric vehicles while training and will also serve as a charging point to newcomers and outside visitors.

Five of the chargers are to be operating in Sofia, two of which have already been installed, while the other two in Plovdiv and Bansko are expected to be operational very soon.

"We always keep on developing and providing new, different and innovative services to our customers. We are pleased to partner with ABB in the implementation of this exclusive project for the users of the service we provide," commented Pulse Fitness & Spa.

ABB's Terra 124 is designed to meet EV battery voltage capabilities up to 920V to deliver charging services across a wider range of today’s and tomorrow’s EVs. The Terra 124 model allows one vehicle to charge at 120 kW or two vehicles to charge simultaneously at 60 kW power each, thus maximizing convenience for drivers. This feature also helps amplify revenue opportunities for the charging operator, as more cars will be able to pass through the chargers, for a significantly reduced time.

ABB is a world leader in electric vehicle infrastructure, offering the full range of charging and electrification solutions for electric cars, electric and hybrid buses, vans, trucks, ships and railways. ABB entered the e-mobility market back in 2010, and today has sold more than 500,000 electric vehicle chargers across more than 88 markets; over 25,000 DC fast chargers and 500,000 AC chargers, including those sold through Chargedot.

ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 105,000 talented employees in over 100 countries. www.abb.com

Links

Contact us

Downloads

Share this article

Facebook LinkedIn Twitter WhatsApp