ABB and Keppel O&M verify next level of vessel autonomy with collision avoidance trials

ABB and Keppel O&M verify next level of vessel autonomy with collision avoidance trials

  • Successful sea trials of harbor tugboat Maju 510 in Singapore verify autonomous collision avoidance capabilities of ABB Ability™ Marine Pilot technology
  • In an industry-first, the vessel developed by Keppel Offshore & Marine receives autonomous notations from American Bureau of Shipping (ABS) and Maritime and Port Authority in Singapore (MPA)
  • ABB’s pioneering digital technology helps relieve the crew of tasks that can be automated, enabling them to perform at their best during critical periods and enhancing the overall safety of operations
ABB in collaboration with Keppel Offshore & Marine (Keppel O&M), has successfully verified autonomous collision avoidance capabilities of ABB Ability™ Marine Pilot technology

Digital technologies from ABB have enabled the harbor tug Maju 510 to become the first vessel in the world to receive Autonomous and Remote-Control Navigation Notation from ABS classification society and first Singapore-flagged vessel to receive the Smart (Autonomous) Notation from MPA. The notations acknowledge the breakthrough performance of the tug, demonstrating autonomous collision avoidance capabilities in trials conducted at Raffles Reserved Anchorage, off Singapore Island, in March 2022.

Keppel Offshore & Marine (Keppel O&M) is the project lead for the autonomous solutions on the Maju 510, which is owned and operated by Keppel Smit Towage, a member of Rimorchiatori Mediterranei. The vessel has already distinguished itself as the world’s first vessel to secure the ABS Remote-Control Navigation Notation, following initial remote operation trials at the Port of Singapore in April 2021. The latest trials verified next level of autonomy, demonstrating automated situational awareness, collision avoidance, and maneuvering control provided by ABB Ability™ Marine Pilot Vision and Marine Pilot Control.

The 32-metre-long harbor tug demonstrated its ability to autonomously avoid collisions in various scenarios, such as when two other vessels approach simultaneously on colliding paths and when a nearby vessel behaves erratically. The trials were supervised by an onboard tug master.

“I had the pleasure of being aboard Maju 510 during the collision avoidance trials and experiencing how smoothly the tug performed in autonomous mode,” said Romi Kaushal, Managing Director, Keppel Smit Towage. “What I found particularly impressive was how the digital system identified one or several risks in the tug’s planned path and responded to set the vessel on a new, safer course. The vessel performed as if it was operated by an experienced tug master.”

By allowing the crew to focus on the overall situation rather than on performing specific maneuvers, the ABB Ability™ Marine Pilot product family enhances safety and efficiency in tug operations, which is particularly important in congested shipping hubs like Singapore, the world’s busiest container port. Furthermore, the systems can be upgraded to enable higher levels of autonomy depending on local regulations and the requirements of the vessel.

“As the systems integrator, Keppel O&M collaborated with ABB on customising the autonomous solutions to enhance the vessel’s operational safety and efficiency. By liberating the crew of time- and energy-consuming tasks and improving accuracy during critical maneuvers, our autonomous solution has proven its ability to increase safety in even the busiest of ports. The autonomous solutions are future-ready to handle the growing demand of tug operations in Singapore port”, said Aziz Merchant, Executive Director, Keppel Offshore & Marine. “Through digitalization, enhanced connectivity, and integrating ABB’s technology, we are able to generate high accuracy positioning and maneuvering, with AI engines for marine object recognition and classification.”

“We are proud to build on our collaboration with Keppel Offshore & Marine and move yet another step closer to making autonomous tugboat operations a reality,” said Juha Koskela, Division President, ABB Marine & Ports. “Our autonomous solutions are designed to support the crew in performing their duties as safely and efficiently as possible. The same technology can be applied to a variety of vessel types including wind turbine installation vessels, cruise ships and ferries.”

In an earlier successful demonstration of ABB’s autonomous technology, the ice-class passenger ferry Suomenlinna II was remotely piloted through the Helsinki harbor. Like Maju 510, Suomenlinna II had been retrofitted with ABB Ability™ Marine Pilot Vision and ABB Ability™ Marine Pilot Control.

Most, if not all vessels could benefit from a higher level of automation for improved safety, efficiency and sustainability of operations. Optimized maneuvering helps to prevent accidents, enhance productivity and reduce fuel consumption and emissions.

The Maju 510 tug performing autonomous navigation – Image credit ABB
The Maju 510 tug performing autonomous navigation – Image credit ABB

ABB’s Process Automation business is a leader in automation, electrification and digitalization for the process and hybrid industries. We serve our customers with a broad portfolio of products, systems, and end-to-end solutions, including our # 1 distributed control system, software, and lifecycle services, industry-specific products as well as measurement and analytics, marine and turbocharging offerings. As the global #2 in the market, we build on our deep domain expertise, diverse team and global footprint, and are dedicated to helping our customers increase competitiveness, improve their return on investment and run safe, smart, and sustainable operations. go.abb/processautomation

ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 105,000 talented employees in over 100 countries. www.abb.com

Links

Contact us

Downloads

Share this article

Facebook LinkedIn Twitter WhatsApp