- Children are playing a key role in accelerating the switch to electric cars, an ABB E-Mobility study for World EV Day has found
- Nearly 60% of parents reported being educated on environmental issues by their children, with over two-thirds discussing EV purchase plans with them
- One-third of US parents who drive an EV said it was pressure from their children which made them make the switch
- Despite growing desire, almost half of parents said that their employer’s policies did not support the switch to driving electric
Children are already driving the EV revolution, despite not yet being able to get behind the wheel themselves, a new global survey has found. Conducted by world leader in EV charging solutions, ABB E-Mobility, the survey revealed that children not only educate their parents on environmental issues and admonish them for un-eco-friendly behavior, but also contribute to discussions around major purchases such as electric vehicles.
The study, comprised of 2,500 parents (with children aged 8-16) and 2,500 children (aged 8-16), involved participants from ABB E-mobility’s 10 largest markets; Canada, China, France, Germany, Netherlands, Norway, Sweden, Switzerland, UK and USA.
Its key findings, released on World EV Day, demonstrate the crucial role that the next generation has to play in helping reduce emissions and enable a more sustainable future.
Speaking about the results of the survey, Frank Muehlon, CEO for ABB E-Mobility, said: “On World EV Day, it is encouraging to see the results of our global study reveal the excitement and determination of young people, as well as the increasing dialogue and action across generations, to move toward a low-carbon future.
“It is also clear, however, that many people still do not feel empowered to take the climate-conscious steps they are clearly ready for. It is our hope that those in positions of power will work together to quickly implement electrification policies which enable a cleaner, greener society, just as we have committed to doing with our ABB Sustainability Strategy 2030.”
With nearly 8 out of 10 parents (79.2%) and three-quarters of children (73.6%) considering the current global environmental situation to be bad, the survey revealed a good deal of intergenerational interaction over the causes of climate change and the steps towards mitigating it.
To that end, almost half of children have told their parents to be more environmentally friendly, while 58.1% of parents said that they have been educated by their children on environmental issues.
68% of children said they are excited about driving electric in the future, with 82.6% (rising to 94.6% in China) stating they intend to drive electric (52.4%) or hybrid (30.2%) when they are old enough.
With 80% of children responding that they believe they have the ability to influence their parents’ purchasing decisions over big ticket items like changing the family car, it is perhaps unsurprising that 78.6% of parents said they would switch to an electric or hybrid model if they were to buy a new car in the next three years.
In the US, this influence was most evident, with 33% of parents who drive an EV saying it was pressure from their children which made them make the switch. Globally, the fact that EVs and hybrids are both better for the environment and more economical ranked as the two highest purchase drivers for current EV owners at 66.1% and 61% respectively.
This rose to 93.8% of parents in China, who also said owning an EV was a better financial investment as well as a more sustainable choice. The nation, which leads the way in EV development, adoption and infrastructure demonstrated its more mature electric market in many of the categories surveyed, with both children and parents reporting far greater awareness of, discussion about and excitement for the benefits of e-mobility.
Other topics covered in the survey further revealed both the momentum towards e-mobility and areas in which work remains to be done. Almost 8 out of 10 parents (98% in China) said that having an EV charger – such as ABB’s Terra AC wallbox - installed would make them more likely to buy a property, demonstrating the importance of facilitating easy and convenient charging.
Room for improvement remains, however, with almost half of parents (48%) also revealing that their company’s policies do not support a switch to EVs. As the International Energy Agency (IEA) projects that EVs will represent 30% of vehicles sold globally in 2030, it is expected that charging at home and the workplace will be critical in meeting much of the overall demand, in addition to a ninefold expansion of public chargers to over 15 million units by the end of the decade.
With the next generation already excited about the journey to electrification, and their parents increasingly coming on board, it is vital that older generations in positions of influence catch up and take the bold decisions needed to support change now.
For its part, ABB has committed to transitioning its entire global fleet of more than 10,000 vehicles to EVs by the end of the decade as part of its 2030 Sustainability Strategy. In the last year alone, the number of charging stations installed at ABB sites increased by almost 100%, from 545 to 1,082. These are split globally across 146 locations in 27 countries. Additionally, in 2021, EVs or plug-in hybrid vehicles (PHEVs) accounted for 44% of ABB's global new vehicle orders.
ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 105,000 talented employees in over 100 countries. www.abb.com
— | ||
Communications | ||