Customer & requeriments
Exolum is the leading company in storage, transport and distribution of petroleum products in Spain. Exolum own oil pipeline network of 4.000 km., which permits the transportation of products from refineries up to the different storage and distribution centers. Exolum also gives services to airports, ports and land markets.
Exolum and ABB began more than twenty years ago their relationship. In 1994 Exolum decided to evaluate a project in the ‘Plant Dispatching’ to improve local operative system and to report in real time and safe way information to the company management systems.
ABB solution
In May 1995 Exolum & ABB Industry System started the project. More than ten years later based on the positive results of ABB, Exolum decided in 2007 to upgrade the system of all loading terminals installations to the new 800xA system platform. ABB offered to Exolum a reliable, powerful and flexible solution based on the new system, it allowed them to centralize the control and the supervision of the different terminals, managing the project according to the new needs of Exolum, ABB progressively replace all the existing subsystems in each loading terminals.
As a result of this joint effort between ABB and Exolum in this project, ABB has received orders for 43 terminals, with a total of 220 loading bays, more than 875 loading arms and tank farms with a capacity of more than 8 million cubic meters of products.
Scope of the project
Exolum required that the functionality in the new platform should fulfill the existing high operational security level demanded, maximum availability of the terminals, remote maintenance, simplicity to configure and upgrade. Besides this functionality, the impact to the operator and the swap time between former system and new system had to be reduced to a minimum.
What our new system offered to Exolum?
- Additive measurement and control of additive mixing.
- Operation control overall terminal balance and statistics.
- Steam recovery and effluent control.
- Direct access to have real time information about situationof orders, trucks, etc.
- Carrying out level and temperature corrections within 800xA platform calculated from data of stream gages.
- Integration of auxiliary services (electrical, fire detection…)
- Remote dispatching which permits supervision and control of all loading terminals simultaneously form Exolum Control Center in Madrid, receiving the information in real time.
Note: We reserve the right to make technical changes or modify the contents of thisdocument without prior notice. With regard to purchase orders, the agreedparticulars shall prevail. ABB AG does not accept any responsibility whatsoeverfor potential errors or possible lack of information in this document. We reserveall rights in this document and in the subject matter and illustrations containedtherein. Any reproduction, disclosure to third parties or utilization of its contents– in whole or in parts – is forbidden without prior written consent of ABB AG.