The key to operator effectiveness

The new generation of high-performance human machine interfaces with
integrated alarm management are improving operator decision-making and achieving significant increases in plant availability

In the era of big data and the Internet of Things, power plants have the capacity to produce more data in a single day than they did in a month 10 years ago. Intelligent equipment, smart devices and sophisticated control systems continuously monitor plant performance, producing a constant flow of measurements and readings on every asset in the plant. But if this data is not provided in context, it can result in information overload and lead to poor decision-making, production loss and reduced profitability.

Staff in all parts of the power plant are dependent on speedy access to the information they need when they need it, none more so than the plant operators. The challenge for HMI vendors is to provide staff - and operators in particular - with the information they require to make correct and timely decisions, while excluding all the information they do not need. The new generation of high-performance HMIs is designed to do this.

Customized and contextualized information
ABB’s S+ Operations HMI, for instance, combines fast, intuitive navigation with simplified gray-scale graphics and integrated alarm management to eliminate information overload and heighten operator awareness. It allows users to personalize their overview of the plant process, so that they can immediately gain access to the information they need.

Closely related to personalization is contextual navigation, through which different user groups like operations, engineering, maintenance and management can access graphic displays and information that are optimized for each group. This enables them to collaborate more easily in their own user-specific environment and share relevant information with colleagues.

Gray-scale graphics
It is no exaggeration to say that the human machine interface is the key to operator awareness. Conventional graphics like the one on the left use different colors to highlight different states or parts of the process. It may be colorful and attractive on the eye, but it provides the operator with far too much information. Each color has to be looked at and its meaning interpreted, a process that can take several seconds. Far more efficient are gray-scale graphics like the one on the right, which reserve color for alarms and abnormal situations. The operator sees the color instantaneously and can respond immediately.

Detecting abnormal situations
High-performance graphics also provide operators with easy recognition of plant and product health. This enables each operator to maintain the process at higher performance levels, leading to real economic gains for the plant owners. Research underscores this point, showing that operators are five times more likely to detect abnormal situations before an alarm occurs with the new generation of high-performance HMIs than with conventional graphics. Once an alarm is triggered, operators solve the problem in about half the time than with traditional interfaces.

High-performance HMIs not only make abnormal situations immediately visible on the screen, they also significantly reduce the number of alarms that vie for the operator’s attention. The maximum number of alarms that the human mind can deal with is just seven, give or take two in a given 10-minute period. Unfortunately, as seen in table 1, operators are bombarded with a constant stream of alarms. In the power industry alone, operators typically deal with 2,000 alarms per day and 350 in a 10-minute peak alarm period. It is therefore not surprising that operators become ambivalent to the constant drone of alarms, tending to ignore 'nuisance' alarms and run the plant on instinct. Clearly, operators cannot do their job effectively when critical alarms are inter-mixed with hundreds or even thousands of non-critical or nuisance alarms.

Eliminating unnecessary alarms
Standards like EEMUA 191 and ISA SP 18.2 have long recognized the need to reduce the number of alarms to match the operator’s cognitive capacity. In this way, the operator is focused and able to act on critical alarms when they occur. High-performance HMIs like S+ Operations have advanced alarm handling and analysis tools that support implementation of alarm management strategies based on EEMUA 191 and ISA 18.2 requirements, thereby ensuring that each alarm generated will alert, inform and guide the operator to take the proper action. An advanced alarm management strategy should fulfill the following objectives:
- The purpose of an alarm system is to direct the operator's attention to plant conditions requiring timely assessment or action;
- Alarms should be presented at a rate that operators can deal with;
- Each alarm presented to the operator should be useful and relevant to the operator; and
- Each alarm should have a defined response.
 
Case studies in cost savings
There are scores of examples and customer testimonies of how measures to improve operator effectiveness have increased productivity and reduced operating costs. Here are two examples from ABB’s portfolio of case studies.

In example 1, a gas plant improved control room operations and corrected its record of poor alarm management. Missed alarms, among other operational and ergonomic issues, were singled out as a major contributor to compressor trips that resulted in downtime and lost production. Fixing the problem reduced the compressor trips from 27 to 7 over a one-year period, saving an estimated $2 million.

Example 2 is a study of plant operators that measured and compared their situational awareness in a conventional distributed control system environment against one in a high-performance HMI environment using simplified gray-scale abnormal situation graphics and integrated alarm management. The figures in table 2 speak for themselves. They translate into estimated cost savings of $ 800,000 per year.
 

 

EEMUA

O&G

PetroChem

Power

Other

Average alarms per day

144

1,200

1,500

2,000

900

Average standing alarms

9

50

100

65

35

Peak alarms per 10 minutes

10

220

180

350

180

Average alarms / 10 minute interval

1

6

9

8

5

Distribution % (Low / Med / High)

80/15/5

25/40/35

25/40/35

25/40/35

25/40/35

 

Table 1: Average number of alarms in selected industries (source: MatrikonOPC)

 

Task

With traditional HMI

With high performance HMI

Result

Detecting abnormal situations before alarms occur

            10% of the time

            48% of the time

                 %x increase

Success rate in handling abnormal situations

70%

96%

     26% over base case

Time to complete abnormal situation tasks

18.1 min

10.6 min

              41% reduction

 

Table 2: Comparison of operator effectiveness in a conventional DCS environment and one using high-performance HMIs

HMI

Links and downloads

Appllication
Symphony Plus
  • お問い合わせ

    ご質問内容などをご入力の上、お送りください。 担当者より折り返しご連絡いたします。

    お問い合わせ
Select region / language