Digital twin applications

digital-twin-abb

Digital twin buzzword demystified

A digital twin is a complete and operational virtual representation of an asset, subsystem or system, combining digital aspects of how the equipment is built (PLM data, design models, manufacturing data) with real-time aspects of how it is operated and maintained. The capability to refer to data stored in different places from one common digital twin directory enables simulation, diagnostics, prediction and other advanced use cases.

Share this page

A typical modern industrial device already creates a formidable digital data-trail. This includes CAD drawings and simulations during the design phase, information on location, connected equipment and configuration from the integration phase, as well as subsequently collected utilization, diagnostic and maintenance data. In addition to such definable, measurable or observable data, algorithms can calculate or simulate non-observable parameters, both actual and predicted.

These data and algorithms typically already exist in various locations or formats. If they could be accessed from one virtual directory – the digital twin – this would provide a comprehensive digital image of the physical equipment. More than being just a static description, this information can be used to simulate the behavior of the physical object. 3-D visualization tools also allow virtual inspection and observation of the equipment and enhance understanding and insight.
The digital twin allows the consistent collection and distribution of information across the physical asset’s complete lifecycle to maximize business outcomes, optimize operations and investment (for both customer and ABB) through data processing (eg, simulation, advanced analytics).

Digital twin applications

Design: Simulation and visualization during the design phase can be used to verify and inspect the overall 3-D design and make sure all parts fit together. Simulations include mechanical, thermal and electrical as well as interrelationships between these aspects.

System integration: 3-D visualizations on a system level can verify constraints such as spatial footprint and physical connections. By connecting to the digital twins of other components, interactions can be simulated, including data transfer and control functionality as well as mechanical and electrical behavior and what-if scenarios. Integration effort on site and the associated downtime for the customer is reduced.

Diagnostics: Observation of the digital twin, for example in a 3-D visualization, can support troubleshooting. Virtual-reality glasses can provide field technicians with an overlay over the real equipment to visualize parameters. Simulations can add non-observable data, such as temperatures of non-accessible parts or material stress.

Prediction: Past and present operational and sensor data in combination with predictive algorithms provide insights into the condition of equipment and the likelihood of different failure modes. This helps plan rational maintenance and reduce unplanned downtime.

Advanced services: If all the advanced service parameters (IoT connectivity, analytics algorithms, etc) are preconfigured in the digital twin, they can be enabled when the equipment is installed and the customer subscribes to these services. In the optimal case, no further engineering is required.
The key to the diverse aspects of a digital twin is the capability to refer to data stored in different places from one common digital twin directory. The digital twin is capable of providing the data required for the different use cases by accessing data from elsewhere in the product lifecycle.
A digital twin supports and removes uncertainty during design and configuration while supporting applications and ensuring availability and reliability through condition monitoring and advanced services.

Shaping the digital future

Taking a leap into the future of industry today, ABB is developing a unified, cross-industry digital capability – extending from device to edge to cloud – with devices, systems, solutions, services and a platform that interacts optimally together. ABB Ability delivers just that capability. Moreover, ABB has embarked on the next step, to create a digital representation of sensors, devices and systems – a digital twin – practically an identical copy of the physical devices.

The digital twin requires a consistent data model that contains the measured variables and the mapping that leads to a digital representation. This function requires that measurements easily reach the digital twin representation, which in turn, necessitates the engineering of a communication infrastructure. To be an adequate approach, this sophisticated infrastructure must be tailored to the digital twin and its unique object. ABB fosters this approach to breakthrough digital industrial technologies at its global corporate research centers.

A few examples

Learn more

Digital transformation partnership: you think big, we get practical.

For every industrial operation ambitious about Industry 4.0, ABB has built a framework to help drive and manage a complex change.
  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language