PROFIBUS DP

PROFIBUS is one of the most used fieldbus protocols. Since its first introduction new features have been added and today there are three protocol variations (DP-V0, DP-V1, DP-V2). ABB drives support two of these variations: PROFIBUS DP-V0 and DP-V1

Our offering includes different PROFIBUS fieldbus adapters depending on the drive type:

 

  • FPBA-01 is compatible with ACS580, ACS480, ACS380, ACH580, ACH480, ACQ580, ACS355, ACSM1, DCS880, DCT880 and ACS880 drives
  • RPBA-01 is compatible with ACS550, ACH550, DCS800 and ACS800 drives

 

Adapters