Panel Builder 600 V4.5 and ABB Ability™ Automation Builder engineering suite


Panel Builder 600 V4.5 is part of the Automation Builder software download which you can find via the following link. Your existing project can be updated easily to Panel Builder 600 V4.5 by opening Panel Builder 600 V4.5 and following the instructions.


Update from BSP V1.0 to V1.3

To be used with Panel Builder 600 V4.5

 

Working with the latest Panel Builder 600 V4.5 requires BSP V1.3 on your CP600. If this version is not already installed, just download the file for your panel via the link below. Unzip it on an USB stick and copy the files to the root folder of the USB stick. Plug the USB stick in the CP600 and the update will start automatically. The USB stick must have FAT or FAT32 format.


Downgrade from BSP V1.3 to V1.0

To be used with Panel Builder 600 versions up to V4.0

For using a CP600 with a Panel Builder 600 version lower than V4.5.0, a BSP downgrade to BSP V1.0.x must be done. We recommend using an USB stick with the dedicated auto-update file which you can download below. Download the file, unzip it on an USB stick and copy the files to the root folder of the USB stick. Plug the USB stick in the CP600 and the downgrade will start automatically. The USB stick must have FAT or FAT32 format.

Application Notes and Examples

You are looking for step by step guidance for engineering or commissioning? You would like to see some example projects?

Go to the Application Examples Selector, filter for subject “engineering” and topic “CP600” and you will find the latest documents.
We collected some questions that might come up during and after your Panel Builder 600 and BSP update.

Operating Instructions

Additional Software