Field Information Manager software download

Download free software - FDI-based fieldbus device management tool

ABB Field Information Manager is the first FDI-based software for device management that makes the configuration, commissioning, diagnostics and maintenance of fieldbus instruments easier and quicker than ever before.

このページをシェアする

FIM page-785

Hardware and software requirements

Supported HART FSK-modems

The free version of Field Information Manager (FIM) contains the ifak modem driver and is already prepared to support ABB/ifak HART modems listed below:

  • ABB NDA121-NX USB (Ex ia)
  • ABB NHA121-NO USB
  • Ifak system isHRT USB
  • Ifak system isHRT USBeX
  • Ifak system H@RT BluePack

Other modems require a manual modem driver installation which is described as a “how to…” in the help file of Field Information Manager.

After a successful installation the help file is accessible on the Field Information Manager main page right upper corner via the “?” button.

Operating System Requirements

  • Windows 7 (32/64bit), Windows 8.1
  • Minimum of 1 Gigabyte RAM.

Installation Guidelines

The free version of Field Information Manager requires user administrator rights to run the installation.

Please start the setup file “ABB Field Information Manager 1.0 DWE (version).exe”  with a right mouse click (or a long finger touch for a touchable device) and select the menu item “run as administrator”.

The setup procedure will guide you through the installation process.

Normally, the installation will complete in less than 3 minutes.

On nodes where ABB Asset Vision Basic software is already installed, it is required to uninstall the “is HRT CommDTM v2” ifak communication driver.

The Field Information Manager setup will install the Microsoft .Net framework automatically if not available.

During installation a reboot might be required. After the reboot please start the FIM setup file again.


Accessing Help

The online help system is accessible on the Field Information Manager main page right upper corner via the “?” button.


Free trial objective

The user is free to use the 1.1 version without ordering a license from ABB. Without a license the tool is designed to connect & configure Online with one HART device at a time via a HART modem.
  • お問い合わせ

    ご質問内容などをご入力の上、お送りください。 担当者より折り返しご連絡いたします。

    お問い合わせ
Select region / language