800xA APC for industrial steam power plants

Advanced process control (APC) using straightforward design and deployment of model predictive control (MPC) with System 800xA DCS enables higher level of automation and optimization of steam power in industrial plants

In several process industries (oil and gas, pulp and paper, minerals, etc.) production requires both steam and electrical power. In these cases, plant operators often build in an in-situ utility unit to satisfy these needs. These are not mainstream power plants like those normally built for power generation. Indeed, not only is the steam needed at different, very specific pressures and temperatures, but its consumption rate is also highly variable due to the variability of the process conditions, trips and/or starts of steam consumers, etc. It follows that steam network stability and reliable power output are difficult to attain.

In some cases,steam is generated also via energy recovery from other units eg, furnaces in a steam cracker or from byproduct gas usage eg, blast furnace gas for a steel manufacturing plant. This introduces further disturbances to the steam network as energy and fuel recovery is subject to upstream unit’s availability and cycles.

Typically the foremost important goal is delivering enough steam, at the required parameters, to the process while producing as much power as economically optimal at a given market conditions. In other configurations, the problem might also comprise delivering heat to a district heating system.



Further complexity is added by energy market variables, prices, and local rules for energy markets. In addition to that, internal incremental production price depend on variable fuel block prices. It follows that in many cases the optimal power output is very different between peak and low energy prices and thus repositioning of the power production is needed. For instance, when the real time energy price is below the internal production price the tie line import is maximized. But when the real time market price is higher than the internal price, the tie line is minimized.

From an APC point of view, typical actuators are boiler rates, steam turbine inlet / extraction rates, gas turbine MW targets, attemperators, pressure control valves, steam flows to users and vent valves.

There are multiple constraints and couplings, delivering a text book case where APC can outperform classical control schemes, typically based on cascades of PIDs and separate PIDs operating with staggered set-points.

Projects of this sort have been executed by ABB quite often in recent years and have delivered a more stable and reliable steam supply to the process with, reduced operating costs, higher energy efficiency, higher average profit (eg, by selling more at higher price and less at lower price) and lower disturbances to the power plant and energy users


APC steam power plant

サポート或いは製品の購買情報をお探しですか?

Learn more

Optimization with APC
Model predictive control technology
  • お問い合わせ

    ご質問内容などをご入力の上、お送りください。 担当者より折り返しご連絡いたします。

    お問い合わせ
Select region / language