The embodiment of reliability for variable speed drives

Day after day our body has to withstand stresses, and as we get old it's only natural that things like our joints start to wear out. Some people such as extreme athletes even push their bodies to the limit, risking broken bones or ruptured muscles when stresses get too high. Understanding the physics of failure (PoF) and predicting the consequences has been keeping medical professionals busy for generations, but these principles don't simply apply to the human body.


Kari Tikkanen, ABB Reliability Engineering Manager, explains how being able to envision the optimum variable speed drive (VSD) for any given application and to understand how the drive will perform over a period of time under certain conditions is akin to analyzing how our bodies will perform over a lifetime. Despite the negative connotations, understanding the physics of failure leads to a healthier future both for the human body and for drives.

From reaction to prediction


Understanding the physics of failure contributes to our success. It's all about moving from reaction to prediction. Much like in sports science, top athletic coaches monitor every step their athletes take in order to predict how the body will behave under stressful conditions. Damage to the body sustained while engaged in extreme physical exertion was considered as a random occurrence and analysis was made using statistical methods with little knowledge surrounding what impacted upon the statistics. This was the same way variable speed drives were previously monitored. Today, predicting failure and reacting before it can have a diverse effect on productivity has become the number one priority.

Statistical Reliability Engineering


Reliability engineers often use the familiar bathtub curve (Image 2) when describing how failure rates behave as a function of time. In this curve the failure rate decreases when the product is new, the failure rate is constant or flat during product’s useful life and increases when the product is getting closer to the end of its design life.


Bathtub curve describes how failure rates behave as a function of time.

The bathtub curve is useful when planning spare parts logistics and making warranty provisions etc. Unfortunately this statistical bathtub model gives you very little information about a new product. The general statistics are not very useful from an individual user’s point of view because their applications and conditions vary a lot. The bathtub curve doesn’t give answers about what to expect when conditions change and what needs to be done if you want to get better reliability. 

A statistical approach is widely used by the insurance industry and economists. Luckily physicians don’t use this method when you ask their advice on how to live a healthy life. They understand that behind the statistics are individuals who have their own stresses and genome that influence what to expect. If the prediction doesn’t match your expectations physicians try to influence it according to the underlying variables.

Two reasons for failure - Two kinds of products


There are only two reasons why products fail: overstress and wear-out. If the stress exceeds its strength the product will fail and the result is an overstress failure. Wear-out failure happens when the cumulative stress exceeds the product’s durability.

There are two kinds of products: nominal and defective. A nominal product doesn’t fail at nominal stress and it will last the useful life it was designed for when exposed to the specified stresses. A defective product fails when nominal stress is applied to the defect site.

It must be noted that if a product is defective it may not fail. It fails once stress is applied to it. In reality there are many more defective products than failures because in most applications the stresses applied are less than they are designed for so the defects remain unnoticed. 

Physics of Failure reliability engineers go beyond the statistics and try to understand the strength of the product and application stresses that influence its reliability. Stresses that influence reliability are temperature, temperature change, humidity, humidity change, voltage, corrosion, vibration, mechanical shock and radiation.

A new look for the bathtub curve


The statistical bathtub curve shows a high failure rate when the product is new. This is typical even if the product is 100 percent tested at the factory before shipment. How can we explain this? 

The PoF approach may give some hints: Two reasons - overstress and wear-out - and two kinds of products - nominal and defective. By analyzing the stresses during the first months or years after shipment it can be easily seen that the stresses that the product experiences before its normal use may exceed the stresses during factory testing. During transportation and storage the product may be exposed to vibration, mechanical shock, humidity and corrosive gases. During commissioning abnormal mechanical stress might be applied on connectors or printed circuit boards, and wrong connection settings can cause excess voltages or temperature changes. Some of these stresses may exceed the product’s nominal strength, and they certainly cause the defects to result in failure.

Once the extra stresses of early life are over and the defective products have been repaired, we enter the phase where failures look random even though in reality they are also caused by overstress like electrical overvoltage, loss of cooling etc. or there was a latent defect that became visible over time. 

When the product is getting old failures get more common. In applications where the stresses are high products will experience shorter life than applications with more moderate stress. In mining, for example, huge shovels are used to fill enormous trucks in just two scoops. As the shovels are under immense strain in extreme conditions, the lifetime of the equipment may be reduced.

It is important to understand that during the whole product life cycle the stress has an impact on the expected reliability as shown in Image 3. All products, nominal and defective will follow the same laws of physics and the same reliability models can be used to predict their future performance.


Impact of stress on reliability.

Image-1-Kari-Tikkanen-ABB-Reliability-Engineering-Manager-390x195

Kari Tikkanen, ABB Reliability Engineering Manager, explains the physics of failure.

Understanding the cause of failure


Even if the product is designed perfectly, failures may happen. When trying to find the reasons for the failure, a thorough root cause analysis needs to be done. What was the cause of the stress and was the product defective or nominal? Before this is known no corrective actions can be taken. Depending on the root cause the actions may be completely different. With this in mind, ABB works closely with our customers to provide consultancy in case of a drive failure and to ensure that the right actions are taken.

Fortunately, tools widely used in medicine also aid root cause analysis in various industrial fields. 3D X-rays, acoustic scanners and SAM microscopes are everyday tools that are used in the ABB’s drives failure analysis laboratory.

Future diagnosis 


The future in drives is exciting. The most sophisticated drives can already predict failure before it happens and in the future they will be smarter still. Intelligent control systems in drives, smart sensors and other innovative services will 'self-diagnose' potential challenges before they arise and not just within the drives, but also in the equipment they are connected to.

Data and diagnostics will also undoubtedly play a larger role than ever before in helping to improve and verify reliability. However, understanding the physics of failure is the first, and most important step, in successfully managing the reliability of variable speed drives.

Reliability testing done in ABB Drives laboratory.

Reliability testing done in ABB Drives laboratory.

Find out more

Related links

Share this page

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language