ABB drives help ensure vegetable quality

ABB’s advanced drive technologies provide precise, on-site and remote environmental control for potato and onion storage, that helps ensure vegetable quality and reduce shrinkage, while saving energy.

Share this page

Company founder Joel Micka says: “Each potato and onion variety has its own temperature and humidity requirements for optimum quality and our systems need to hold very accurate settings – within a tenth of a degree – to allow food storage up to 12 months.”

To achieve this, JMC uses ABB standard drives to control fan-motor speed and airflow, keeping temperature and humidity at precise settings. Incorporating drives enables the fans to run more
efficiently by matching air volume precisely to demand. When air demand decreases, the variable speed AC drive slows the motor down, saving energy and helping farmers maximize their sales margins.

In a typical installation, used in an onion store, six 18.6 kW/25 hp drives use about 19.2 kWh at 100 percent speed. If the fans are reduced to 50 percent speed in the winter, when storage volumes are down and the outside temperatures are low, each of the fans use about 2.8 kWh. All six fans at 50 percent speed use less energy than one fan at 100 percent speed. If the six fans are kept at 50 percent during a one month period, savings of 70,848 kWh or $5,667 per month can be made.

Remote control improves safety and efficiency


Even more important than the energy savings is the safety and efficiency the new systems provide through remote control and monitoring, because storage facilities are often located many miles from the main offices. Says Micka: “With the old systems using traditional motor contactors, if the motor current increased to a level that was too high, it would trip and shut down the motor and then shut down the whole system until someone checked on the building and restarted it.”

With the optional intelligent ethernet module, the drives can be monitored remotely, either through a modem or via the Internet, allowing faults to be quickly diagnosed and solved, without the need to visit the storage site. Communications can be set up to send an alert via e-mail to the operators to warn them when a fault trip occurs. JMC integrates all of the systems components, refrigeration units, fans, drives and doors, into a network operated through a remotely accessible control panel.
jmc onion storage

JMC Ventilation Refrigeration specializes in the design and manufacture of custom ventilation and refrigeration systems for potato and onion storage. JMC’s high-tech storage facilities use ABB drives to keep farm produce fresh.

Facts

Customer FR Sistems of Bagnolo Mella
Location Washington State, USA
ABB deliveries   ABB drives to control ventilation fans to optimize temperature and humidity conditions
Keys to success Energy savings, vegetables can be stored for up to 12 months without a reduction in quality, remote control of drives via optional intelligent ethernet module allows fast and efficient solution for problems

Find out more

Damansara City_view_small
Read the article
Damansara­ City­ upgraded ­by­ a ­Cool ­Solution
  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language