IEEE-PES GTD Asia 2019

Place and date

BITEC, Bangkok , Thailand

-

Add to calendar ICal Outlook Google Calendar

IEEE PES GTD Grand International Conference & Exposition Asia 2019
Conference: March 19-23 | Exposition: March 21-23


Overview

The IEEE-PES Thailand Chapter is proud to be hosting the IEEE-PES GTD Grand International Conference & Exposition Asia 2019 (IEEE-PES GTD Asia 2019) from 19-23 March 2019 in Bangkok, Thailand.

This conference is an extension of the 40th year for "IEEE-PES T&D Conference and Exposition", which is the largest conference and exposition on Power & Energy being held biannually in North America. This will be the first time the conference is being held outside the USA and the Local Organizing Committee in Thailand is confident in bringing new facets and valuable inputs to the international community of power & energy.

http://ieeegt-d.org/