TruONETM makes sure data flows when primary power doesn’t

GettyImages-580501779_super_v2_550
The world’s first true all-in-one ATS enhances critical power security for data centers.

The new TruONE is the world’s first true all-in-one automatic transfer switch, engineered 
to incorporate switch and controller in one seamless unit. Performance tested beyond standard 
requirements, TruONE stands ready to ensure the steady delivery of critical power at all times.

Continuous Operation
Say goodbye to blinking lights and stopping motors. TruONE provides a fast in-phase open transition of power, guaranteeing unnoticed generator use during business hours. 

Safety and Protection
TruONE enables emergency manual operation—even under load—without opening the panel door when the HMI is mounted to the ATS frame. The HMI can be detached from the frame for door mounting, offering more flexibility for the panel designer. Best of all, regardless of the HMI installation method, there’s no need for connecting dangerous line voltages to the door, so the risk of operator injury due to equipment malfunction is reduced.

Check how TruONE allows emergency manual operation for immediate power restoration Link to YouTube.

Data and connectivity
TruONE features cloud-based connectivity through the ABB Ability™ Energy and Asset Manager.  ABB Ability simplifies implementation and use of TruONETM in coordination with other ABB devices, ensuring one common user interface and one common software environment. Market-leading modular connectivity with seven communication protocols ensures easy installation and connectivity now and far into the future.

Learn more about AbilityTM  Energy and Asset Manager.
FS_Webpage_banner_customer

Tools and Support

Documents browser

Select region / language