Architecture

ABB showcases a further evolution in the low-voltage distribution business, setting a new benchmark in terms of simplicity and performance.

ABB Ability™ Electrical Distribution Control System enables the collection of relevant information from the ABB de­vices installed in the low-voltage power distribution system. 
These devices can be connected, plug & play, to the cloud-computing plat­form by sharing data either with Emax 2, Ekip UP and TruONE™ (equipped with Ekip Com Hub) or with Ekip E-Hub via Modbus RS-485 or Modbus TCP.

Embedded solution
External solution
Upgrade solution

Embedded solution with Ekip Com Hub

Emax 2 equipped with the new Ekip Com Hub establishes the cloud connection for the whole switchboard.
This dedicated cartridge-type communication module just needs to be inserted into the terminal box and connected to the internet.

External solution with Ekip E-Hub

The Ekip E-Hub module can be mounted on DIN rail to collect data throughout the system.Moreover, it is possible to connect sensors for environmental parameters (temperature, water, gas) via both analog and digital I/O. Modules for Wi-Fi or GPRS connection are provided as optional features.

Upgrade solution with Ekip UP

Ekip UP equipped with Ekip Com Hub establishes the cloud connection for a specific feeding line, load or even for the whole distribution system. This dedicated cartridge type communication module just needs to be inserted into the terminal box and connected to the internet using an external router.

Discover more

Overview
Ease of use