Web story 2019-01-15 ABB’s TruONE automatic transfer switch helps Puerto Rico regain reliable power As hurricane-ravaged Puerto Rico struggles to restore crucial power, the island’s only electric generator manufacturer is relying on TruONE for easy assembly and service.
Web article 2019-01-15 Power protection for the semiconductor industry Low- and medium-voltage power protection solutions from ABB help to prevent significant losses from voltage events
Web article 2019-01-11 ABB technology helps SENA expand solar homes in Thailand Adoption of solar rooftop technology is allowing villagers to reduce the energy taken from the grid and lower the cost of their electric bills
Press release 2019-01-10 ABB launches a single-phase UPS for industrial applications up to 80 kVA reducing the total cost of ownership The modular UPS has a high current rating, giving a superior short-circuit performance that is ideal for selectivity and fault clearing in critical industrial applications.
Web article 2019-01-10 Thesis work better than any job interview Gurudeep Manjulgud Devraj’s thesis work paved the way to full-time employment. Now he is part of ABB in Kungsbacka.
Press release 2019-01-09 ABB Powers-up Service Crew at Dakar Rally 2019 with Solar Energy Working in close collaboration with its partner, SoliTek, ABB’s efficient REACT 2 solar storage solution, has been installed as part of an off-grid solar installation on the Craft Bearings multipurpose Service truck. The set-up is being used to harness enough solar energy during the day to support the service and ancillary team as they undertake essential repairs to the race cars at night, as well
Web story 2019-01-09 ABB parts help the Coronel Brothers prep for another grueling Dakar Rally Ty-Rap® cable ties and Shrink-Kon® connectors will help ‘The Beast, Part Two’ challenge one of the world’s toughest off-road treks
Web story 2018-12-07 ABB technology enables Siam Cement Group to harness the sun’s energy ABB’s PVS800-57 central inverters enhance solar power production from a 25 MW ground-mounted solar system
Web story 2018-12-06 A home for all seasons When it comes to creating a welcoming environment at home, the Danish have long led the way with their ‘hygge’ concept. With up to 17 hours of darkness per day in the depths of winter, and average temperatures hovering around 0°C, the Danes have made crafting cosy bolt-holes into an art form. And while creating this sense of warmth and refuge from harsh weather traditionally relied on open fires,
Web story 2018-12-05 ABB's ruggedized UPS protects industrial applications with the beneficial concept of modularity ABB’s UPS innovation is enabling manufacturers to integrate technology designed for clean rooms with dusty production floors.