LKAB's underground mines are among the most high-tech in the world. Safe and resource-efficient production with well-developed production methods and processes is crucial for profitability.
The Kiruna mine site consists of eight mine hoists in the central mine hoist facility (CA), and another five at the sub-level. Over the years, ABB has delivered equipment for all 13 hoists.
Being the main artery in LKAB's production flow, the mine hoists in the CA facility transports the ore from the sub-level (898 m) up to ground level. For this generational upgrade project, ABB has delivered mechanical equipment for the mine hoisting facilities and shaft, electrical and control equipment as well as electrical installation, installation supervision, construction management and commissioning.
The project, which was started in 2014, has been running for over a decade and was finalized in 2025 on time and below budget and will ensure productive and safe operations for at least another 25 years.
“The solutions we have put in place have been designed around the need to future-proof one of the world’s largest and most productive mines", says Björn Jonsson, Global Business Line Manager, Hoisting, ABB. "Working closely with LKAB, we have delivered an upgrade that ensures the flexibility necessary for the long-term success of operations for at least the next quarter of a century.”