ABB showcases VD4-AF, a new vacuum circuit breaker for steel furnaces at ACW China

ABB showcases VD4-AF, a new vacuum circuit breaker for steel furnaces at ACW China

High-performance features enable relentless operation and protection for steel furnaces at lower costs

ABB enhances its portfolio in China with the launch of medium-voltage circuit breakers with VD4- Arc Furnace, a unique solution based on vacuum technology and innovative actuation systems, to provide a new high quality, reliable and efficient solution.

The VD4-AF circuit breaker, which performs up to 150,000 close-open operations, ensures zero downtime for breaker overhaul thereby reducing total costs of the furnace operation. The embedded control unit enables optimized operations with servomotors, increasing the circuit breaker’s performance by up to ten times of what could be previously achieved.

“We recognize the steel manufacturer’s daily challenges to boost output and increase utilization levels of assets,” said Matteo Caiti, Global Product Group Manager, Control and Protection Products for ABB. “The VD4-AF solution enables their operations to run continuously to produce the highest quality product.”

The VD4-AF circuit breaker is designed with a draw-out, roll-on-floor construction, to be combined with the ABB PowerBloc enclosure. This allows a faster and easier integration or replacement operation. This together with the 150,000 close-open operations result in more than a 50 percent reduction to the frequency and duration for inspection or maintenance, compared to any other solution.

Additional features include:

  • Embedded advanced diagnostics
  • Up to 38 kV, 2500A, 31.5 kA
  • Built-in interlocks

Join us at ABB Customer World China 2018 on November 14 and 15 at the Xiamen International Conference and Exhibition Center, Fujian Province. Detailed information about VD4-AF circuit breaker, its advantages and main features is also available at the product webpage.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in power grids, electrification products, industrial automation and robotics and motion, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner in ABB Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 147,000 employees. ABB has a full range of business activities in China, including R&D, manufacturing, sales and services, with 18,000 employees located in 142 cities, 40 local companies, and online and offline channels across over 300 cities.

For more information on ABB, please visit: http://new.abb.com/cn

ABB Digital Marketing Center: https://mall.abb.com.cn    Sina Weibo: @ABB Electrification Products          Official WeChat Account: cnabblp 

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp