Let's unravel HVACR complexities with Tim R. Skell!
Our expert, Tim R. Skell, spent almost 3 years sharing his expertise in the #FunFactFriday series on LinkedIn. Now, we are giving him a forum to exchange news, knowledge, and passion for HVACR technologies in the new ABB column.
Join the discussion with Tim R. Skell on LinkedIn to read other fun facts and share ideas!

Most HVACR drives have a real-time clock that tracks date and time, and it is typically used to provide a date/time stamp for each drive fault occurrence. This info can be helpful in troubleshooting, i.e. does this fault happen around the same time every day?
How about some lesser-known fun facts about the ACH580 clock:
- Events are also date/time stamped – i.e. when exactly did that high static safety open?
- Battery backup as standard (no extra accessory required).
- The clock uses BACnet to automatically sync up with the BAS/BMS clock.
- It enables scheduling for start/stop and setpoint (day of week, time, season, holidays).
- The clock supports daylight savings (on/off) and adjustable start/end date of daylight savings.
- You can select between 12- or 24-hour style clock.
- It has flexible date format - (mm/dd/yyyy), (dd/mm/yyyy), or (yyyy/mm/dd).

Having a clock, along with the supporting features that take advantage of the clock, allows a mini-automation system to live in the drive. This can either supplement your existing automation system or allow standalone operation.