About ABB:s partner program
The ABB Value Provider Program is a global network of trusted partners, including distributors, wholesalers, panel builders, installers, service providers, system integrators, and OEMs. These partners, known as ABB Value Providers, are accredited by ABB and meet high standards for service and support. When you work with an ABB Value Provider, you get the same level of expertise and objective advice as you would directly from ABB, along with the added benefit of local knowledge and experience. This partnership ensures top-quality support and service, helping you achieve your business goals.
Enhanced Service Capacity and Expertise
By including Elektroautomatik in the Service Partner Program, ABB Robotics can further strengthen its service capacity and ensure that customers receive the best possible service. Elektroautomatik has a total of 200 employees, including 40 service technicians based at four sites: Kungsör, Södertälje, Gothenburg, and Skövde. The company has invested in training for service technicians at ABB in Västerås and in special tools to perform certifications and component replacements on ABB robots. They also offer customized training programs on-site in Skövde, where they have three ABB robots, and can send robots and personnel to customers for training.

The expanded program allows ABB's partners to offer service agreements and extend the lifespan of automation investments, such as through robot upgrades. By monitoring customers' robots and informing partners when replacements are needed, ABB enables customers to benefit from proactive service and maintenance. This leads to increased cost efficiency and sustainability for the end customer.
Urban Gustavsson, Business Unit Manager at Elektroautomatik, says:
"It is fantastic to be able to leverage ABB's expertise in this collaboration. This enables us to deliver even better service to our customers and ensure optimal performance for their robots."

Long-term Collaboration and Quality Assurance
To ensure high quality and standards, ABB has developed an onboarding program where partners are certified. Elektroautomatik has been a reliable partner to ABB since the 1990s. With extensive experience in automation dating back to 1965, Elektroautomatik has completed many successful installations. The company offers comprehensive services for entire automation systems, including new installations, long-term service, upgrades, and improvements. Now, Elektroautomatik is also a certified service partner, further enhancing their capacity to provide high-quality support.
Customer Benefits
ABB's monitoring of installed robots and spare parts in Sweden provides a complete overview of the status of all installations. This enables partners to inform customers when replacements are needed, reducing production risks and increasing cost efficiency. "We work together to be proactive," says Urban Gustavsson.
Currently, a project is underway with Elektroautomatik where four robots are being replaced in an existing production line. This 15-year-old automation solution is being upgraded by replacing only the robot systems, while the rest of the installation remains intact. This approach avoids replacing the entire automation line, minimizing production downtime and costs. This method is particularly beneficial for production-critical facilities as it requires only a short stoppage.
Thomas Johansson, Sales Manager for Service and Aftermarket at ABB Robotics, describes the collaboration as a groundbreaking solution in Sweden:
"For the end customer, this is a way to protect their automation investment. They receive advance notice of when a replacement is needed, minimizing the risk of production stoppages. This collaboration provides the best possible service with local support."

About Elektroautomatik
Elektroautomatik is Sweden's largest automation integrator and a comprehensive provider of automation solutions. The company offers customized automation solutions, AGVs, high-quality machines, training, and services that streamline and ensure the quality of customers' production and logistics. With expertise from idea to finished production and a broad range of competencies, Elektroautomatik is a complete partner for sustainable and innovative solutions.