ABB unveils new open drip-proof (ODP) motors at Turbomachinery & Pump Symposium 2025

ABB unveils new open drip-proof (ODP) motors at Turbomachinery & Pump Symposium 2025

ABB, a global leader in electrification and automation, is proud to announce the launch of its latest line of open drip-proof (ODP) motors at the Turbomachinery & Pump Symposium (TPS), taking place September 16-18 at the George R. Brown Convention Center in Houston, Texas, U.S. Attendees are invited to visit booth 2617 to experience firsthand how ABB’s innovations are driving performance, reliability and energy efficiency in industrial motor applications.

The new ODP motors, in NEMA frame sizes 5000 and 580, are optimized for 460V/60Hz operation and engineered to deliver exceptional power density and cooling performance, making them ideal for demanding industrial environments. Designed with IE3 efficiency (equivalent to NEMA Premium Efficient), these motors help reduce energy consumption while maintaining robust performance in applications with moderate exposure to dust and moisture. These motors can also be configured as WPII or IP44 motors (without a bonnet) due to an innovative design with a series of internal right angles and filters that provide additional protection in outdoor environments.

Key features of ABB’s new ODP motors:

  • High power density without the need for auxiliary cooling
  • Superior energy efficiency for reduced operational costs
  • Reliable performance in challenging industrial conditions
  • Compatibility with existing North American motor installations for easy retrofits and upgrades

Robert Boyce, U.S. Division Manager for IEC Low-Voltage Motors, will be available at the booth for scheduled interviews and technical discussions. Visitors will also learn about ABB’s broader portfolio, including the Baldor-Reliance® SP4™ Super Premium motors, EC Titanium™ integrated motor-drive units, and the full range of ABB SynRM motors, all designed to meet the evolving needs of the compressor and pump industries. Click here to schedule an interview with Robert.

“The launch of our new ODP motors reflects ABB’s commitment to innovation and sustainability,” said Robert Boyce. “We’re excited to showcase how these motors can help our customers achieve greater efficiency and reliability without compromising on performance.”

Event details:

Turbomachinery & Pump Symposium 2025

  • Dates: September 16–18, 2025
  • Location: George R. Brown Convention Center, Houston, Texas, U.S.
  • ABB booth: #2617

ABB Motion, a global leader in motors and drives, is at the core of accelerating a more productive and sustainable future. We innovate and push the boundaries of technology to contribute to energy efficient, decarbonizing and circular solutions for customers, industries and societies. With our digitally enabled drives, motors and services we support our customers and partners to achieve better performance, safety and reliability. To help the world’s industries outrun – leaner and cleaner, we deliver motor-driven solutions for a wide range of applications in all industrial segments. Building on over 140 years of domain expertise in electric powertrains, our more than 22,000 employees across 100 countries learn and improve every day. go.abb/motion

ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and more than 105,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com   

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp