ABB meets the needs of the water industry in Mexico with NOM/ANCE-certified Vertical Hollow Shaft motors

ABB meets the needs of the water industry in Mexico with NOM/ANCE-certified Vertical Hollow Shaft motors

[Ver] la versión en español

ABB has expanded the availability of its industry-proven Vertical Hollow Shaft (VHS) motors to meet the growing needs of the water industry in Mexico, supported by newly obtained NOM/ANCE certification. Designed specifically for vertical pumping applications, ABB VHS motors are engineered to deliver reliable performance across critical industries including agriculture, mining, municipal water, wastewater treatment and industrial processing.

With NOM (Normas Oficiales Mexicanas) and ANCE (Asociación de Normalización y Certificación) certification, ABB VHS motors are compliant with Mexico's regulatory requirements for safety and energy efficiency, enabling customers, equipment manufacturers and channel partners to confidently specify and deploy ABB solutions across the country.

ABB VHS motors are purpose-built for vertical pumping systems, offering a combination of durability, serviceability and application-specific design advantages:

  • Simplified maintenance – Top-mounted coupling design allows easier access to pump components, reducing downtime and service complexity
  • Operator-preferred features – Integrated sight glass enables quick visual inspection of thrust bearing lubrication
  • High-thrust capability – Engineered to handle demanding vertical loads in deep well and high-capacity pumping systems
  • Rugged construction – Available in multiple enclosure types, including weather protected and totally enclosed designs for harsh environments
  • Drop-in design – Built to standard NEMA dimensions for seamless replacement and retrofit

As demand for water infrastructure, irrigation systems and industrial pumping continues to grow in Mexico, ABB's expansion of its pump motor portfolio supports the need for reliable, efficient and serviceable motor solutions.

“ABB's practical, reliable Vertical Hollow Shaft motors aren't just engineered for performance - they're designed to help Mexico tackle its water crisis,” said Sam Harris, Executive Vice President, Fluid Dynamics and Heavy Industrial Solutions, ABB. “With reduced energy consumption, extended service life and simplified maintenance, our motors enable customers to operate more sustainable, cost-effective pumping systems that support Mexico's long-term water security."

Understanding NOM and ANCE certification

Official Mexican Standards (NOM)
Normas Oficiales Mexicanas (NOM) represents mandatory technical regulations issued by Mexico's standardization agencies. These standards establish rules, specifications and guidelines applicable to products, processes and services to promote quality and economic development. Products complying with NOM standards may use the official NOM seal, regulated by Official Mexican Standard NOM-106-SCFI-2017.

ANCE certification
The Asociación de Normalización y Certificación (ANCE) is a Mexican standards and certification organization specializing in electrical, electronics and telecommunications products. ANCE provides conformity assessments for NOM and NMX standards, ensuring products meet Mexican safety, efficiency and quality standards for legal sale in Mexico. Key aspects of ANCE certification include comprehensive testing at authorized laboratories to verify safety and regulatory compliance, focus on electrical products and equipment performance standards, verification of manufacturing quality and product consistency and ongoing auditing to ensure sustained compliance.

The achievement of the NOM/ANCE certification represents a significant milestone for ABB's expansion into Mexico's pumping market. These certifications remove regulatory barriers, allowing ABB to serve Mexican customers with confidence. They enable equipment manufacturers and channel partners to confidently specify ABB VHS motors without compliance concerns, positioning ABB as a trusted partner committed to meeting Mexico's stringent quality and safety standards and supporting growing demand across agriculture, municipal water systems, industrial processing and mining industries.

ABB Vertical Hollow Shaft motors are backed by the company’s global expertise in motors and drives, combined with strong regional support. The introduction of NOM/ANCE-certified products reinforces ABB's commitment to enabling local customers with solutions that meet both performance expectations and regulatory standards.

VHS motor key features

  • NEMA Premium (IE3) efficiency delivering consistent torque and energy savings
  • Extra high-thrust capacity with 175% extra thrust on 440 frames and above
  • Stationary and non-reverse ratchet preventing reversing due to backspins
  • Standard NEMA P-base flange allowing easy drop-in replacement Inverter-duty rated for compatibility with modern variable speed drives
  • Top-mounted coupling for easy shaft and pump access
  • Heavy-duty cast iron frame, UL listed and weather protected
  • Wide range of configurations from 15-500 horsepower with multiple voltage and frame options

ABB Motion, a global leader in motors and drives, is at the core of accelerating a more productive and sustainable future. We innovate and push the boundaries of technology to contribute to energy efficient, decarbonizing, and circular solutions for customers, industries, and societies. With our digitally enabled drives, motors and services we support our customers and partners to achieve better performance, safety and reliability. To help the world’s industries outrun – leaner and cleaner, we deliver motor-driven solutions for a wide range of applications in all industrial segments. Building on over 140 years of domain expertise in electric powertrains, our more than 22,000 employees across 100 countries learn and improve every day.  new.abb.com/motion

ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and more than 105,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com   

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp