ABB launches Grinding Connect to accelerate digitalization of gearless mill drives

ABB launches Grinding Connect to accelerate digitalization of gearless mill drives

  • New service suite brings together ABB’s key digital grinding capabilities into a single platform, enhancing visibility of critical mine operations
  • Grinding Connect builds on ABB’s expertise from more than 160 gearless mill drives sold worldwide
  • The suite is designed to optimize performance, extend equipment life, ensure uptime and reliability, and enable data-driven decision-making

ABB today announced the launch of Grinding Connect, a new digital service suite for mining companies operating gearless mill drive (GMD) systems. Available globally, the new suite is designed to improve visibility across critical grinding assets, reducing unplanned equipment downtime and supporting more efficient maintenance planning at a time when mines face growing pressure to maintain throughput and reliability.

Grinding Connect is developed to address the need for more remote expert support, maintenance and continuous performance, through a single cloud-based service suite built specifically for ABB GMD systems. The suite leverages ABB’s knowledge from more than 160 GMD projects worldwide, which is combined with secure cloud analytics and service workflows to allow users to view system conditions, access service records, submit service requests, and interact with ABB expert support through one platform.

With demand for critical minerals expected to triple by 20301, according to the International Energy Agency, mining companies are under pressure to scale and stabilize the production of critical materials. Continuous performance and reliability of large grinding circuits are critical to plant output, with unplanned downtime estimated to cost up to $500,000 an hour according to ABB research2.

  • With Grinding Connect in place, everything is connected. Image ABB
  • The launch of Grinding Connect is a next step for digitalization in grinding processes. Image ABB
  • Mining operators can look forward to even more practical ways to improve equipment availability, reduce response times and make better-informed decisions. Image ABB

The service suite brings together digital solutions that ABB has introduced to the market over recent years, including Asset Health and Condition Monitoring analytics, Trendex diagnostics and troubleshooting as well as GMD Copilot, ABB’s AI‑powered virtual support assistant. Within Grinding Connect, mining operators can access prescriptive maintenance recommendations, supported by more than 180 trend signals as well as alarms, events, transient recording integration and signal correlation.

The platform is also designed to provide anomaly detection, frozen-signal detection and smart notifications, alongside recommended actions from ABB experts to support continued operation. By supporting remote diagnostics and expert collaboration, the suite reduces the need for reactive on-site intervention, helping service teams to prioritize actions more effectively.

“Mining operators are looking for practical ways to improve availability, reduce response times and make better-informed decisions for the maintenance of production-critical assets,” said Mikel Torre, Global Business Unit Manager Grinding, ABB’s Process Industries division. “Grinding Connect brings ABB’s service and GMD system knowledge into one digital environment, meaning users can work with a complete view of asset condition, service history and expert support. Only with this level of visibility will operators make progress towards the industry transition to increasingly autonomous, more efficient mining operations.”

Grinding Connect has been developed in line with ABB cybersecurity standards and IEC 62443-related product development practices, including penetration testing during verification. It is available globally for mining customers using ABB gearless mill drive systems.

1. Critical Minerals – Topics - IEA

2. Industrial downtime costs up to $500,000 per hour and can happen every week | News center | ABB

ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and around 110,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com

ABB’s Automation business automates, electrifies and digitalizes industrial operations that address a wide range of essential needs – from supplying energy, water and materials, to producing goods and transporting them to market. With its ~26,000 employees, leading technology and service expertise, Automation helps process, hybrid and maritime industries outrun – leaner and cleaner. go.abb/automation

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp