- New ABB SureWave Static Frequency Converter (SFC) provides seamless clean power for marine vessels when in port
- Reducing CO2 emissions and energy costs for global shipping industry
- SureWave SFC will help ship owners avoid fines and taxes by switching their diesel generators off in port
Clean and highly efficient, ABB’s new SureWave Static Frequency Converter ensures the static, seamless, and automated transfer of power from a ship’s onboard generator to an onshore power source, removing the need to use diesel burning generators when in port. Switching to this next generation of static conversion technology will enable ship owners to avoid fines and taxes imposed for not using shore power once berthed.
ABB has engineered SureWave SFC to be 50 percent smaller than previous models and for added flexibility, it can be installed on the marine vessel or port side. To further increase energy efficiency and reduce carbon emissions, ABB’s SureWave can be paralleled or connected to renewable energy sources like PV or wind farms. As frequency and voltage can vary between ports around the world, SureWave SFC allows more flexibility when connecting 60 Hz powered equipment to a 50 Hz supply network or 50 Hz powered equipment to a 60 Hz supply network. In addition, using a power module smart enough to operate as an inverter or rectifier, makes maintenance, stocking, and servicing stress free.
ABB’s SureWave is accredited with the PEP ecopassport, an assessment aligned with the UN sustainability program and ISO 14025 and ISO 14040 to verify a product’s environmental performance. The accreditation considers materials, production, transportation, usage, and end of life. ABB’s SureWave scored class-leading results across its lifecycle due to its superior efficiency and design.
“The shipping industry is under increasing pressure to reduce global carbon emissions and its environmental impact. Many ports are introducing penalties for ships using diesel generators when they are docked. By switching to next generation static conversion technology like SureWave, operators can avoid charges and significantly lower CO2 emissions and noise pollution during their stay,” said Sebastien Surply, Global Product Group Manager for ABB Power Protection. “During SureWave’s estimated 15-year lifetime, shipyard owners and operators could expect to reduce their CO2 emissions by approximately 350 tons and deliver operational cost savings to port stakeholders in the region of 1.4M USD1, when compared to traditional rotary systems.”
Thanks to its modular design, SureWave SFC from ABB can cover a variety of power sizes. Scalable from 250 kVA up to 2.25 MVA for a single system, it is the ideal solution for small to medium port and ship-yard installations, as well as a range of marine vessels ranging from super yachts to super tankers. If required, SureWave SFC can also support higher loads up to 10 MVA with multiple system parallel connections. SureWave SFC also provides market leading overload and fault clearing capabilities and low distortion. Distortion caused by unoptimized power supplies can result in harmonics, unbalance, and low power factor, which lead to higher electricity bills and potential damage to electrical infrastructure.
For more information on ABB’s SureWave register your interest for our upcoming webinar – “Next Generation of Sustainable and Reliable Shore-Power” here (https://campaign.abb.com/l/501021/2022-02-10/wlvktk) , or visit https://new.abb.com/power-converters-inverters/grid-interconnections/industrial/surewave
Notes to Editors:
1 Savings ($) calculation is based on a comparison against rotary FC with about 80 percent efficiency. For savings generated by less cooling, a SEER (seasonal energy efficient ratio) of 13 was used. The application selected was Shipyards, with a profile of 8 hours per day and 5 days a week, for a 2.25MVA system.
ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 105,000 talented employees in over 100 countries. www.abb.com
ABB’s Electrification Business Area is a global leader in electrical products and solutions, operating in more than 100 countries, with over 200 manufacturing sites. Our 50,000+ employees are dedicated to transforming how people live, connect and work by delivering safe, smart and sustainable electrification solutions. We are shaping the future trends of electrification, differentiating through technological and digital innovation while delivering an outstanding experience through operational excellence for our customers across utilities, industry, buildings, infrastructure and mobility. For more information visit https://go.abb/electrification