The future is already here

The digital power plant of the future is already possible and ABB can deliver it

The industrial Internet is about connecting machines with people and services. It is about harnessing big data, analyzing that data and turning it into actionable information. It is about optimizing the plant and production process and about making equipment and service smarter. And, it is about improving collaboration to enhance the expertise of the people who operate, maintain and manage it.


The digital power plant embodies the industrial Internet to achieve those objectives. It has five main qualities:

Ever-young

  • Continuously learns from the past to improve efficiency
  • Has a technology foundation that evolves, never becoming obsolete
  • Allows continuous and flexible DCS upgrades
  • Lives longer and healthier, thanks to intelligent predictive maintenance

Aware and self-sufficient

  • Is aware of its operating status, all the time
  • Knows its operating limits and capabilities
  • Asks for maintenance at the correct time
  • Does more with less - in operations and maintenance

Predictive

  • Knows how much energy it needs to produce to meet market commitments
  • Manages resources optimally in relation to operating status, weather and market constraints
  • Knows when equipment has developed a fault and when it requires repair

Safe and secure

  • Safe for people, the local community and the environment
  • Conscious of its environmental impact, always minimizes emissions
  • Safe for employees
  • Cyber secure

Open and responsive

  • Flexible in relation to market requests
  • Anticipates market requests by forecasting external conditions
  • Open and responsive to owner and grid requirements
  • Can operate within a virtual power pool of renewable and conventional plants


Common platform

The digital power plant of the future is based on a common, open-source platform to facilitate collaboration between people and partners.

Our ABB Ability™ platform, for instance, uses the best industry-standard, open-source and proprietary ABB software. It combines our technology leadership and deep domain expertise with strategic partnerships - with Microsoft to use Azure as our cloud platform, and with IBM to jointly develop artificial intelligence and machine learning solutions for industrial applications.

This approach makes it easier for customers to integrate our solutions with other platforms they may already have deployed. It also enables system integrators that are certified developers on Microsoft Azure, IBM Watson and SAP HANA to create new applications that interoperate with ABB Ability™ solutions.

Such a broad, open and inclusive ecosystem delivers massive benefits to customers, compared to narrow, closed and exclusive proprietary systems.

Closing the loop

The digital power plant of the future closes the loop between data and action.

It is not enough to simply collect and analyze system data; the data have to be turned into actionable information to improve plant performance. Only by closing the loop with an action is value created.

Closing the loop does not only apply to devices and machines, it applies to people and service as well. Bringing them together - people, plant and production process - unlocks new opportunities to reduce downtime, improve energy and equipment efficiency, lower maintenance effort and improve productivity.

Collaborative operations

The digital power plant of the future is built on collaboration - within the plant, fleet and company, and with valued partners and suppliers.

Our collaborative operations center for power generation delivers those benefits. It connects the plant and fleet with company headquarters and ABB, enabling people to work together and improve plant performance.

Through a high-speed, cyber-secure connection to the plant’s distributed control system, the center continuously retrieves and analyzes plant performance data, monitors key performance indicators, delivers actionable information for plant personnel and management, and - when needed - provides deep domain expertise from ABB within minutes.

Fog, cloud and intercloud

The digital power plant of the future uses the 'fog,' cloud and intercloud, together.

Mission-critical automation systems like the DCS and enterprise software systems are traditionally housed on-site, in what is called ‘fog computing.’ New digital solutions will increasingly feature functionality at the fog and cloud level, allowing data and functionalities to migrate from one to the other. This creates increased flexibility in deployment models based on customer preference.

ABB believes that no single IoT platform will provide all the capabilities that customers need. Instead, there will be an ‘intercloud’ of applications that interoperate across multiple IoT platforms. An ABB Ability™ solution will be able to connect to one running on those other platforms, provided that interfaces and data formats are compatible.

Enabler technology and expertise

While others are only recently discovering the value of digital, we have long been experts in integrating digital components into our customers’ control systems. These include sensors, software, digital networks and, now, the power of the Industrial Internet of Things.

We are world leaders in securing and using data via our installed base of around 70 million digitally enabled devices, 70,000 digital control systems and 6,000 enterprise-level software solutions. This expertise and installed base forms the strong foundation upon which ABB Ability™ is built.

THE DCS is key

Hand in hand with our long digital heritage is our 125-year history in power generation and our 100 years in control technology.

Our complete and fully integrated electrical and automation solutions for power plants comprise essential ABB Ability™ digital solutions that continuously provide actionable information on plant equipment, the production process and energy market, enabling the plant to operate optimally and profitably.

The key component in these integrated solutions - and the digital brain of the plant - is our ABB Ability™ Symphony® Plus total plant automation system, the number-one DCS in power generation worldwide, according to industry analysts, ARC Advisory Group.

ABB solutions

Links and downloads

フォローする

LinkedIn
Follow us
LinkedIn
  • お問い合わせ

    ご質問内容などをご入力の上、お送りください。 担当者より折り返しご連絡いたします。

    お問い合わせ