DS Smith's Kemsley mill: A model for secure operations and enhanced connectivity in a digital age

DS Smith Kemsley Mill, Kent, UK smaller

The pulp and paper industry has made real progress by harnessing the power of digitalization and new technologies around the world. While this has revolutionized mill operations and quality control for many, the convergence of information technology (IT) and operational technology (OT) has also caused a notable shift in vulnerabilities to cyberattacks.

Clearly, cyber security is a constant consideration for companies of all sizes, and threats change with technological evolutions. According to Professor Stuart E. Madnick – Professor of Engineering Systems at MIT and Founder of the Cybersecurity at MIT consortium – and Apple, there was a 20% increase in data breaches from 2022 to 2023 with over 360 million instances of corporate or institutional data breaches in the first 8 months of 2023. According to Madnick, these attacks have proven that organizations are only as secure as their ‘least secure link’. Therefore, foundational cyber controls at every level must never be overlooked in efforts to prevent incursions.

A cyber security breach in a pulp, paper, packaging, or tissue mill can bring production to a halt with potentially widespread consequences, even from just a minor breach. One day of lost production or downtime in a mill could cost millions of dollars. There are also many potential sources of indirect loss in the immediate wake of a breach. In the long term, mills must contend with the costs to validate that their systems are back to normal, manage regulatory reporting and invest additional time into rebuilding trust with customers.

New industrial technologies have placed a great emphasis on connectivity. Cyber security efforts in the pulp and paper industry must offer a unified overview of all connected devices, enabling users to patch, protect and analyze security from one central system. ABB recently supported DS Smith to do just that. The two organizations worked together to upgrade legacy systems and establish enhanced cyber security architecture.

 

Stefano2_230412
ShankarSingh
Article by Stefano Cinquina, Global Business Line Manager & Shankar Singh, Global Product Line Manager, Drives & Automation, Pulp and Paper, ABB Process Industries, first published in Paper360 May/June 2024 Edition, available here

Analyzing a generational challenge

DS Smith is a leading provider of sustainable fiber-based packaging worldwide, supported by recycling and papermaking operations. The company’s Kemsley Paper Mill in Kent, UK, has been in operation for 99 years and is today the second largest recycled paper mill in Europe with an annual production capacity of over 820,000 tons.

As it edges towards its centenary, the DS Smith Kemsley team faces a new generational challenge to create highly automated, increasingly connected and more secure operations. As a technology leader with decades of history and many industry firsts in pulp and paper, ABB is embedded in the mission.

For the last decade, an older version of ABB Ability™ System 800xA distributed control system (DCS) was used successfully, but it did not lend itself to effectively supporting the latest technology and hardware. The time had come for a full system upgrade with enhanced cyber security architecture to meet modern requirements.

ABB DCS

Combining safety with automation

Together with a quality control system (QCS), drives and machine control across all three paper machines on the 1.1km2 site, the DCS touches every area of the mill. At such a scale, the idea of a seamless upgrade may have seemed impossible to many.

For the Kemsley mill, cyber security is an important part of its license to operate. The team wanted to maintain their security but recognized the importance digitalization plays now and in the future. Digitalization was a driving force behind this large-scale and complex project, as well as a deciding factor in partnering with ABB.

Tackling the complexities of a large-scale upgrade

ABB and DS Smith worked together over an 18-month period developing a process of design, focusing on architecture and a comprehensive solution to deliver on the goals set by DS Smith. This collaborative approach shaped the solution and ensured an effective planning and testing process, mitigating obstacles and challenges ahead of implementation.

The mill scheduled shutdown on all three paper machines, beginning with PM3 and PM4 simultaneously, followed by PM6 and their effluent and freshwater plant. The team recognized the importance of the project and timed it for minimal disruption to normal operations. Having three paper machines on one site isn’t common within the industry and added to the complexities and logistics of such a project – raising the stakes significantly.

It became one of the largest system upgrades that ABB has supplied into the industry, taking over 6,000 hours in advance and 12 days on site. The team completed a full upgrade of the ABB Ability™ System 800xA distributed control system (DCS), quality control system (QCS) and paper machine drives, with mill-wide integration.

Virtual measurements were also included in the scope of project delivery, adding strength and weight measurements for more accurate and frequent measurements. Additional complexity lay in integrating across the operational technology, implementing cyber secure architecture all the way from automation to control to IT.

 

DigitalPTI

Securing mill-wide operations

 

Mapping out a complex architecture to deliver cyber security at every level of operations, ABB had the expertise and power of both local and co-ordinated resources to deliver a close-to-seamless upgrade.

ABB Ability™ System 800xA is a key operating system for DS Smith and with enhanced integration and more secure options, visibility of operations mill-wide have improved significantly.

 Having a long-standing relationship with the local teams and co-ordinated resource from ABB’s Europe Regional Execution Center (EUREC) was crucial to project success, aiding smoother communication and project management. DS Smith was comfortable putting their trust in the ABB team.

 “Facing a challenging upgrade across a heavily integrated system, we anticipated many obstacles. Thanks to ABB’s time, effort and expertise, we achieved a seemingly impossible seamless upgrade. It has very much prepared the ground for what we want to do in the future,” said Adrian Clark, Electrical and Automation Development Manager at DS Smith. 

 

Takeaways for the pulp and paper industry

For those companies just beginning their cyber security journey in the industry, ABB’s pulp and paper specialists recommend focusing on a three-pronged approach; people, policies, and procedures, working alongside the right technology. The introduction of technology must be matched with operational measures that bring in people and processes. This typically includes defining policies and procedures for utilizing the new technology as well as educating employees accordingly. Foundational level technical and organizational security controls must be in place to defend against the majority of the generic threats, but after that there are multiple layers to consider. Companies must undertake continuous management and maintenance of their controls, possibly choosing to add more sophisticated controls. Cyber security is not a ‘once and done’ project and requires strong collaborative operations for controls with managed security service.

It is important not to shy away from adopting new technologies just because of the elevated security risk. There are thousands of companies around the world that have invested in new networks, smart automation and edge and IIoT technologies that haven’t experienced devastating cyberattacks. This is because they secured against threats by considering and implementing security as part of the overall transformation plan.

Patching and applying updates may seem rudimentary, but they are among the most important things that can be done. It is prudent to have the highest levels of cyber-hygiene. That means having a layered defence strategy in place.

As exemplified by DS Smith's Kemsley Mill, digitalization presents a roadmap for a more secure, efficient, and sustainable future for the pulp and paper industry. By embracing these advancements and fostering collaborative partnerships with industry leaders like ABB, manufacturers can unlock the true potential of digital transformation and secure their competitive edge in the years to come. 

 

PaperRollsPTI

Learn more

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language