Turbine concepts

Utility-scale wind turbines have two main electrical drivetrain concepts: doubly-fed and full converter. The main differences between the two are the type and size of generator used and the function of the converter

Full converter concepts are increasing market share

The market has largely been dominated by the doubly-fed concept, but there are several factors driving a shift toward full-converter, including grid code compliance and optimized power generation at slower wind speeds.

Evaluating concepts

Each of the electrical drivetrain concepts impact the turbine’s weight, size and maintenance needs. Selecting an electrical drivetrain concept needs to be done carefully, weighing the requirements of the turbine with the needed certifications and grid code specifications that apply once the turbine is installed.

Engineering partner

Once the electrical drivetrain concept is selected, expert ABB engineers are available to work with the manufacturer to discuss and integrate ABB products into the turbine engineering drawings, specifications and plans. Turbine manufacturers benefit from ABB’s experience, resulting in design cost savings and increased efficiencies. The following section provides a more detailed overview of each of the electrical drivetrain concepts for use by manufacturers during their concept studies.

Doubly-fed concept
High-speed full converter concepts
Medium-speed full converter electrical drivetrain package
Low-speed full converter electrical drivetrain package
Permanent magnet generator technology
  • Contact us

    Submit your inquiry and we will contact you

    Contact us