LOG IN 🔒: Partners | ABB

Taking Control Room environmental protection to the next level

Personal Air Purifier is a unique solution designed to improve air quality and health in Control Room environments. The system address PH1 particles, which can cause serious respiratory diseases such as asthma, pneumonia and chronic obstructive pulmonary disease, the Air Purifier can be easily integrated into ABB’s Operator Wellbeing Service (OWS) digital platform, and is the latest addition to ABB’s portfolio of solutions designed to improve operator wellbeing, boost productivity and avoid shutdowns.
Personal-Air-Purifier
Globally, air pollution is one of the greatest environmental risks to personal health. Studies show that indoor air can be up to 50 times more polluted than ambient air2. Protecting em-ployees working in Control Room environments is vitally important to keep operators healthy, motivated and productive.

  • Most offices use filters to improve air quality, but these often only remove PM2.5–PM10 particles such as dust and smoke, neglecting more serious PM1 combustion particles, bacteria and viruses3.
  • Air pollution is the second-highest risk factor for noncommunicable diseases (those not passed from person to person). It also causes 6.7 million premature deaths annually4 and costs billions in lost productivity and medical care globally.
  • Are your operators performing at the top of their game? Adverse environmental factors can result in operator fatigue or distraction. Up to 80% of industrial accidents can be blamed, at least in part, on human behaviour, with emergency plant shutdowns often the result of inadequate responses.

Why Personal Air Purifier ?

PM1 Classed in accordance with ISO 16890, the Air Purifier removes up to 60% of all PM1 dust and up to 85% of all bacteria. By improving air qual-ity, the Air Purifier contributes to a healthier work environment. Designed with user convenience in mind, the system is easy to install and re-quires minimal maintenance. This allows you to focus on what matters most – Your Operation.

PAP enables you to:
  • Upgrade your existing ABB Extended Operator Workplace (EOW) solutions
  • Improve indoor air quality and create a better work environment
  • Help protect employees from serious respiratory diseases like asthma and pneumonia
  • Boost productivity, reduce absenteeism and enhance comfort
  • Retain skilled operators and attract new talent

Key benefits:
energy_efficiency
Boost Productivity

Cleaner air leads to sharper focus and higher efficiency.

Healthier-operators
Reduce Absenteeism

Healthier operators mean fewer sick days and more consistent performance.

Air-Purifier
Enhance Comfort

A Personal Air Purifier creates a more comfortable and pleasant working environment.

Related offerings

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language