Power quality conditioning

semiconductor_header

Challenges

Voltage sags and variations and voltage imbalance represent one of the biggest threats to manufacturers and industrial facilities around the world.

Let's see which are the most typical origins and effects of these phenomena.

Voltage sags and variations

Voltage imbalance

Another problem that affects industrial loads is voltage imbalance. The direct impact of this effect on the working life and characteristics of an electric motor is defined in standards such as NEMA Motors and Generators Standard 1 (MG-1). For example, if the voltage imbalance was 3 percent, the motor loading should be derated to 90 percent of its rated load. Excess loading reduces motor life significantly and causes the unit to operate with lower efficiency and, in extreme cases, can cause motors to overheat and burn their windings.

Segments

Key values

Low voltage solutions overview for Power conditioning

Active voltage conditioning Static frequency converters Reactive power compensation

 

 

PCS100 AVC-20 PCS100 SFC PCS100 RPC
PCS100 AVC-40    

For more information

Other solutions

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language