Selectivity

Basic concepts

What is selectivity?

Selectivity
Total selectivity
Partial selectivity

Selectivity

There is selectivity between two circuit-breakers in series when, owing to an overcurrent flowing through both of them, the load-side circuit-breaker opens thereby protecting the circuit, whereas the one on the supply-side remains closed, thus guaranteeing power supply to the rest of the installation.

Total selectivity

Selectivity for any overcurrent value there may be in the installation.

Partial selectivity

Selectivity only up to a certain Is current value (ultimate selectivity value). If the current exceeds this value, selectivity between the two circuit-breakers is no longer guaranteed.
Selectivity_Techniques_home_292x146

Selectivity techniques

The different selectivity techniques, also from the operational point of view.

 

Advantages

 

Tools & Support

 

Special applications

 

Focus on

 

Related offering

 

  • Contact us

    Submit your inquiry and we will contact you

    Contact us