Is-limiter applications to reduce high short-circuit currents

The trend towards higher line kVA ratings and the growing intermeshing of power systems are increasing the likelihood that distribution switchboards will be subjected to unacceptably high short-circuit currents. Reliable and economic protection against these surge currents is provided by the Is-limiter. 

This fast-acting switching device triggers a small charge to open the main conductor, which is designed to carry high operating currents. The current commutates to a parallel fuse with high breaking capacity, which limits the short-circuit current during the first rise. Is-limiters are being used successfully in more than 2.500 stations in 70 countries.

Such a fast switching device caters for a variety of applications which cannot be fulfilled by conventional switches. The most important of these are presented below. See Figure 1 below.

Coupling - parallel operation of two systems

Is-limiters are frequently used in the coupling between two systems or parts of systems whose short circuit withstand capability would not be sufficient with parallel connection via a circuit breaker .

Instead of designing the two systems for double the short-circuit current, an Is-limiter is installed in the coupling. In the case of a fault, it limits the peak short-circuit current at the very first rise. It separates the systems electrically into two parts before the short-circuit current can endanger system components. After separation, only the faulty part of the system still feeds the short circuit, which is selectively shut down by the relevant circuit breaker. The peak short-circuit current thus does not become higher than the short-circuit current from a single transformer at any point in the switchgear. When the Is-limiter trips, the voltage in the part of the system not affected by the short circuit only drops for fractions of a millisecond at most.

Even sensitive loads are thus protected from voltage dips. The Is-limiter is therefore also highly suitable for installation in the coupling between an ”unprotected” an a ”protected” system. See Figure 2 below.

Station service supply and public network
 
More and more frequently, systems for the in-house supply of power, operated in parallel with the public supply network, are encountered in industrial and service operations. If a fault were to occur in the public network, the additional short-circuit current from the station service supply facilities would cause the permissible levels in the utility network to be exceeded.

Figure 2 above shows the most technically appropriate – and frequently also the only – solution: the use of an Is-limiter in the coupling to the public supply network. If necessary, the Is-limiter can respond to a directional tripping criterion. This requires three additional current transformers in the main star point lead of the generator. With the directional tripping criterion, the Is-limiter only trips in response to short circuits in the public supply network. See Figure 3 below.
 
IS-limiter in the generator feeder to protect the high voltage system

Deregulation of the market leads to installation of many additional generators. For this reason the short-circuit currents on the high voltage level will be too high. By using the Is-limiter the high voltage level will be protected against the short-circuit currents fed by these generator feeder. See Figure 4 below.
 
IS-limiters and reactors connected in parallel

If system components are not to be totally isolated in the case of a short circuit, but further supplied via a short-circuit current limiting reactor, the reactor can be bridged by an Is-limiter in normal operation, so as to avoid the copper losses, voltage fluctuations which would otherwise occur during load changes and the electro-magnetical influences causes by each reactor. Figure 4 beside shows Is-limiter and reactors connected in parallel in both incoming and outgoing feeder.

See Figure 5 below.
 
Selectivity with the use of several IS-limiters

When several Is-limiters are installed in a system, additional tripping criteria can provide for selective tripping. In such cases, only that Is-limiter which is closest to the fault location is tripped. Figure 5 below shows this application.

REFERENCES
[1] Dreimann, E.; Grafe, V.; Hartung, K.-H.: “Protective device for limiting short-circuit currents"etz 1 15 (1994) 9, 492-494
[2] Is-limiter, ABB AG Calor Emag Mittelspannungsprodukte, 2000

Karl Heinz Hartung was born in 1945 in Neukirchen. He received the M.Sc. degree in electrical engineering from Technical University in Aachen.Profession: ABB AG Calor Emag Mittelspannungsprodukte, Developing department (short circuit calculation, Is-limiter, electronic test equipment, c.t.s., circuit breakers) since 1992 General Manager for Is-limiter. He is also a member of CIGRE Working Group 13.10 "Specifications for Short Circuit Current Limiters"

Are you looking for support or purchase information?

ABB Connect Partner Hub

ABB Connect Partner Hub is a dynamic online community and offers multiple valuable services for our customers.

Learn more

Get to know more