An open-pit mine reduces conveyor failures and maintenance with a new drive configuration

An ABB gearless conveyor drive (GCD) matched with a low-voltage permanent magnet motor logged a better performance than a conventional drive-and-motor combo during a trial at LEAG's open-pit lignite mine in Cottbus, Germany

Share this page

Customer situation

belt conveyor
  • heavy dependence on high-capacity conveyor belt systems to be reliable, efficient and very robust
  • substantial hourly cost of a conveyor breakdown
  • challenges with the maintenance-intensive gearbox of conventional conveyor drives

ABB's solution

GCDnew

Completely new approach for medium-power applications that fulfills eco-design requirements:

Benefits

  • energy savings
  • reduced failure rates
  • lower maintenance overheads
Peter Scholze, head of services, open pit mines, LEAG
"The interest of LEAG in this pilot project mainly lies in the expectations related to higher efficiency, lower wear and hence less expenses for repairs and maintenance”
Peter Scholze, head of services, open pit mines, LEAG
"Operations and maintenance team found the new system to be easy to learn, understand, and use, without any major difference in operation or handling when compared with the existing systems”
Ulf Richter, product manager, GCD, mining, ABB Process Industries
"During the one year of operation, we measured 6% energy saving and 100% availability of the drive with just two hours inspection”
GCD pilot
GCD medium

Establishing the feasibility of installing GCDs on mobile mining machines and suitability of permanent magnet motor

The pilot project established the feasibility of installing GCDs on mobile mining machines and shows the suitability of permanent magnet torque motors to drive conveyors. The results reveal that on both productivity and energy efficiency metrics, GCDs are viable alternatives to conventional geared drives. The potential for energy savings, reduction of failure rate and maintenance have also been demonstrated. The gearless solution has performed better in regard to dynamic accuracy and overall efficiency than the existing traditional solution.

Leadership at Lausitz Energie Bergbau AG (LEAG), owner of the Jänschwalde mine, which staged the project, lauded the solution. “The interest of LEAG in this pilot project mainly lies in the expectations related to higher efficiency, lower wear and hence less expenses for repairs and maintenance,” Peter Scholze, head of services, open pit mines, LEAG, said. “Since commissioning has taken place, the drive has been running smoothly.”

Further, Jänschwalde’s operations and maintenance team found the new system to be easy to learn, understand, and use, without any major difference in operation or handling when compared with the existing systems.

The proof, according to Ulf Richter, product manager, GCD, mining, ABB Process Industries, is in the numbers. “So far, during the one year of operation, we measured 6% energy saving and 100% availability of the drive with just two hours inspection,” he said.

The gearless solution has performed better in regard to dynamic accuracy and overall efficiency than the existing traditional solution

Enabling exact benchmarking between the conventional and the new drive configurations

The development amounts to historic precedent, Richter said. “This had not been possible to-date from technical and commercial points of view with the existing solution based on synchronous motor technology,” he said. “The key point for success was the decision to use permanent magnet motors.”

Tracing back to research and development initiated in 2013, the GCD package adopted by LEAG in June 2017 also included a frequency converter and a transformer. “The new gearless solution was installed on a high-capacity (15,000 metric tons per hour) discharge conveyor of a bucket chain excavator,” ABB reported.

The low-speed synchronous electric motor is controlled by a variable-speed drive to produce a shaft rotational speed of typically 50 to 150 rpm.

Enabling exact benchmarking, the GCD system runs in parallel to the existing geared drive” on the 2.5-meter-wide belt “located at the end of the discharge boom. Both drives connect to the same pulley shaft. The belt moves sand and large rocks (ice-age foundlings) that give rise to mechanical shock and vibration.

Ambient temperatures reportedly range from -25° to 40°C. And that is what the technology was built to handle, Richter said. “The drives are out in the field without any additional protection” from temperature swings, he said. Mobile or semi mobile conveyors generate higher shock and vibration stress than stationary equipment, he said. And contaminant “ingress must be avoided,” Richter said. “This has all been incorporated in the design of the drive assembly.”

Learn more

conveyors
  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language