- Equipped with Visual SLAM, ABB’s AMR T702 trolley robot offers increased speed, accuracy and autonomy in navigation and logistics.
- Integration with ABB’s AMR Studio software allows new users to easily configure AMR routes and jobs.
- Intuitive Visual SLAM and user-friendly AMR Studio together can reduce commissioning time by up to 20 percent.
ABB Robotics has announced its first Flexley Tug T702 autonomous mobile robot equipped with AI-based Visual SLAM navigation technology and the new AMR Studio software, enabling first-time robot users to easily program and operate entire fleets of mobile robots. The new capabilities simplify configuration and can reduce commissioning time by up to 20 percent, paving the way for a workplace where intelligent robots operate autonomously, amid a critical shortage of skilled labor.
“Following our acquisition of Sevensense in January, I’m pleased we are offering our first AMR with AI-based Visual SLAM technology and AMR Studio software. With this combination in our mobile robotsin our mobile robots, we offer unmatched intralogistics flexibility and scalability for ABB’s customers, in an environment that is shifting from linear production to dynamic networks of manufacturing,” said Marc Segura, President of ABB Robotics. “The AMR T702 is a perfect match for a wide range of industries, such as automotive, consumer goods sector or logistics, especially in large warehouses and fulfilment centres where their surroundings may be constantly changing”.
The latest announcement follows the acquisition of Swiss start-up Sevensense in January as ABB continues to expand its portfolio to meet the growing market for mobile robots, which is expected to expand at a rate of 20 percent CAGR through 2026, from $5.5bn to $9.5bn.1.
Combining AI and 3D vision, Visual SLAM technology enables AMRs to make intelligent decisions, differentiating between fixed and mobile objects in dynamic environments. Using Visual Simultaneous Localization and Mapping (Visual SLAM), the robots can create a map that is used to operate independently, reducing commissioning time from weeks to days and enabling fully autonomous operation in highly complex, dynamic environments alongside people. Maps are constantly updated and shared across the fleet, offering instant scalability without interrupting operations and greater flexibility compared to other navigation technologies.

The new capabilities offered by Visual SLAM are further enhanced by the launch of ABB’s AMR Studio® software (AMR Studio), which enables inexperienced users to easily create and configure AMR routes and jobs, with no programming knowledge needed. AMR Studio® streamlines the process of setting up an entire AMR fleet from start to finish, guiding users through the necessary steps, from environment mapping to mission generation and system configuration.
Once the fleet is up and running, AMR Studio® Fleet Manager software puts users in full control of what is happening on the shop floor. Intelligent order assignment uses powerful algorithms to ensure that orders are distributed efficiently, while real-time visualization and data monitoring provides full traceability.
The software’s flexible, user-friendly user interface also makes AMR fleets more easily scalable by putting users directly in control of system modifications and adding new routes.
ABB will continue to expand its AMR portfolio with Visual SLAM navigation technology and AMR Studio®.
ABB will showcase a T702 equipped with Visual SLAM and AMR Studio at the LogiMAT tradeshow in Stuttgart, Germany from March 19-21, in Hall 6, booth D31. For more information, including a free ticket and registration for the booth tour, visit: ABB Logimat.
1 ABB analysis