Two essential components of household electrical safety
Grounded protection and surge protection serve complementary but equally important roles in home electrical safety. Grounding – also known as earthing – provides a safe path for fault currents, preventing dangerous electric shocks. Surge protection diverts sudden voltage spikes to ground, safeguarding your household electronic devices against costly damage.
Modern Canadian homes require both systems to work together to keep people and electrical equipment safe. Grounding alone won't protect your precious electronic gadgets against power surges; surge protection requires proper grounding to work effectively.
Your Home's Safety Foundation: Understanding Grounded Protection
What does grounding actually do?
Grounded protection is an electrical safety system that routes fault currents to earth, safeguarding people from dangerous or potentially fatal electric shock and reducing the risks of fire and damage to equipment. Grounded protection provides a low-resistance pathway for currents caused by faulty equipment or unsafe electrical wiring. Also known as ‘grounding’ or ‘earthing’, it directs fault currents into the earth via a grounding wire that’s bonded to metal water pipes or a dedicated conducting rod buried in the ground.
The main purpose of grounded protection is to ensure the safety of people and equipment in the event of household electrical faults. By itself, grounding will not protect electrical systems and equipment from voltage surges, for example, caused by lightning strikes. However, it’s an essential component of a comprehensive home safety system that includes voltage surge protection as well as grounding.
How grounding protects you
Imagine what can happen if the insulation of a current carrying wire inside a faulty appliance, like a washing machine, becomes damaged, or if the end of a wire comes loose inside an appliance. If that stray wire makes contact with the metal casing of the device, the whole appliance suddenly becomes live. This presents the serious danger of electrocution for anyone standing in contact with the ground who touches the device.
The human body acts as a conductor, carrying current from the live metal casing, which is at a potential of 120 volts, to the ground, which is at a potential of zero volts. That current flow from the appliance through the body to ground can cause serious injury, and even be fatal.
Grounded protection provides an alternative route. It allows excess electrical energy from live parts of the appliance to take the path of least resistance to earth, leaving people unharmed. As this excess energy flows to earth via the grounding connection, it may also trigger a circuit breaker to trip or a fuse to blow. This halts the flow of current and isolates the device, rendering it safely inoperable until the root cause of the problem is identified and fixed.
Proper grounding protection is required by the Canadian Electrical Code for all residential properties.
What grounding doesn’t protect
While the primary purpose of grounding is to give protection against electrocution, it doesn’t provide a complete electrical safety solution by itself. Grounded protection alone won’t prevent sudden voltage surges – caused by lightning strikes to incoming power lines, faulty household wiring, using EV chargers or domestic appliances – from reaching sensitive electronic equipment and potentially causing costly damage.
This is where surge protection plays an essential complementary role. It ensures that transient over-voltages – sometimes lasting milliseconds or less – are safely diverted away from the electronic gadgets in the house, allowing them to operate smoothly and safely without the risk of damage.
Understanding Surge Protection: Defending Your Electronics
What does a surge protection device (SPD) do?
A surge protection device (SPD) deals safely with sudden voltage spikes that can damage or destroy household electronic devices. There are several causes for voltage surges in Canadian homes. It’s important to remember that not all surges are dramatic one-time events. The sensitive electronics inside household devices can be stressed by smaller voltage fluctuations over time, impairing the performance of your home tech and shortening its life.
What causes power surges in Canadian homes?
Lightning strikes to overhead power lines or transformer equipment are a common occurrence in parts of Canada that are prone to thunderstorms, especially during the summer months. This can cause sudden voltage spikes, as can other grid issues or the restoration of the mains supply after a power outage.
Within the home, surges may be caused by the use of EV chargers or simply by switching heavy-duty appliances like refrigerators or HVAC systems on and off. Power surges can also be caused by domestic circuits being overloaded when too many devices are plugged in, as well as by old or damaged household wiring.
What do surge protection devices protect?
Think how many electronic devices there are in the typical Canadian household. These can include:
- ICT, including computers and servers, Wi-Fi hubs, data storage and other home office equipment
- Entertainment systems, TVs and gaming consoles
- Smart home devices and IoT equipment
- Kitchen appliances with electronic circuit boards
- HVAC, home automation and building access control systems
All these devices and systems may contain microprocessors and other sensitive electronics that are at risk of damage from voltage surges, requiring costly repairs or replacement. Proper installation of surge protection devices by a licensed electrician is the surest way to protect your investment and keep all your home tech running smoothly.
What’s required for surge protection?
Residential surge protection requires installation by a qualified electrician of a surge protection device (SPD), normally on the main household electrical panel or at a service entrance. However, that’s only half the story. An SPD also requires a proper grounded pathway to operate. Without grounded protection, there’s no way for excess voltage detected by the SPD to be dissipated safely to earth.
And that’s why ensuring grounding and surge protection to current CEC regulations are both vital parts of providing adequate electrical protection for Canadian homes, including new and refurbished properties.
Read our article: What Is Whole Home Surge Protection - And Is It Worth It?

Why ‘Grounded Or Surge Protection?’ Isn’t The Right Question
Partners, not alternatives
The purposes of grounding and surge protection are commonly confused, causing a misapprehension that one or other system provides adequate safety protection for your household’s occupants and electronic devices. This is analogous to asking whether your house needs foundations or a roof: both are essential partners for ensuring the structural integrity of your home.
The answer to the question “which system do I need in my own home?” is “both”. The roles of grounding protection and surge protection are complementary. Grounding exists primarily to protect people from the danger of electric shock.
However, grounded protection alone cannot deal with transient over-voltages due to lightning strikes or other causes that can damage home gadgets.
By contrast, surge protection helps safeguard your household electronics. Although it won’t work without a proper grounding pathway that allows excess voltage spikes monitored by the SPD to dissipate safely to earth.
The cascade effect: Whole-home protection strategy
Effective electrical protection follows a cascading approach, where each layer builds upon the one before it. At the foundation is proper grounding, which is essential for basic electrical safety and provides the pathway needed for excess electrical energy to be safely dissipated.
Building on this foundation, the most significant step homeowners can take is installing whole-home surge protection. A surge protective device installed at the service entrance or main electrical distribution panel acts as the primary defence against damaging voltage spikes. By intercepting surges before they spread through branch circuits, whole-home surge protection safeguards wiring, appliances, and connected electronics throughout the house.
For homeowners who want to go a step further, point-of-use surge protectors, such as power bars with built-in protection, can be added at sensitive devices.
In this cascading approach, grounding enables protection, whole-home surge protection does the heavy lifting, and point-of-use devices offer additional refinement, working together to deliver more complete, reliable protection than any single measure alone.
Real-world scenarios: When you need both systems
Scenario 1: Lightning strike nearby
Lightning strikes to overhead cables and power transformers are a common consequence of electrical storms that are prevalent in regions of Canada, occurring most commonly in the summer. Lasting just milliseconds or even less, the electrical energy in a high-voltage lightning strike can nevertheless be more than enough to damage or destroy delicate household electronic circuitry.
Safeguarding your home against lightning strikes requires the combination of properly specified and installed surge protection, with an effective grounding system that allows transient voltage spikes to dissipate safely to earth without endangering people, equipment or household wiring.
Scenario 2: Appliance short circuit
An exposed or damaged wire carrying mains voltage inside an electrical appliance will cause a short circuit if it comes into accidental contact with the device’s metal casing. In this situation, the whole of the appliance now presents an electrocution risk if it’s touched. Proper grounding prevents this, causing this dangerous fault current to flow harmlessly to earth and tripping a circuit breaker or blowing a fuse.
An SPD on its own doesn’t provide protection against fault currents and accompanying shock hazards. Nonetheless, the SPD does require a grounded pathway to divert momentary voltage surges to earth.
Scenario 3: Utility grid switching event
Not all voltage surges are dramatic one-time events. There can be smaller but regular fluctuations in mains supply voltage during normal supply operations. Over time, these frequent surges can put stress on the delicate electronic circuitry inside modern household gadgetry, compromising its performance and shortening its lifespan.
Installing surge protection – with proper grounding – will smooth out these everyday fluctuations in household supply voltage, optimising the performance of all your electronic equipment and maximizing its working life.
Canadian Electrical Code Requirements
What does the CEC require?
At a basic level, the Canadian Electrical Code (CEC) requires all residential homes to have proper electrical grounding and bonding in place. This is a fundamental safety measure designed to protect people from electric shock and help electrical systems operate safely.
The Code also recognises surge protective devices and sets out rules for how they must be installed and connected when they are used. However, whole-home surge protection is not currently required for every residential property under the base CEC.
Because the CEC is adopted and enforced at the provincial and local level, requirements can vary depending on where you live and the type of electrical work being done. For that reason, while surge protection isn’t universally mandatory, it’s widely regarded as a best-practice upgrade, especially for modern homes filled with sensitive electronics and smart devices. A licensed electrician can confirm what applies to your specific home or project.
Choosing the Right Surge Protection for Your Grounded Home
Does your home need electrical panel upgrades?
Surge protection for all your household circuits and devices is normally provided by the installation of an SPD on the main household electrical panel or at the service entrance. Typically, modern SPDs such as ABB's CSA/cUL-certified THOMESURGE and THQLSURGE2 can be readily installed by a qualified electrician without requiring any special modifications or upgrades to the panel itself.


Verifying your home's grounding system
For true peace of mind, there’s no substitute for enlisting the help of a licensed electrician to check the condition of your property’s grounding system. As well as identifying potential improvements to your grounding arrangements, this can also help maximize protection of all your household electrical systems with advice on specification and installation of a high-quality SPD.
Don’t delay getting professional help if there are any telltale signs of problems with your property’s grounding system. These can include frequent circuit breaker trips, flickering lights, or a tingling sensation when touching poorly or unearthed appliances.
Installation considerations
Checking your grounding system while adding surge protection can be a practical, cost-effective upgrade for homeowners. A licensed electrician can assess both at the same time, ensuring the surge protective device (SPD) is installed correctly and connected to a properly grounded electrical panel.
What to expect during installation
In most homes, installing a whole-home surge protection device is a straightforward job. The electrician will typically start by inspecting the main electrical panel and grounding system to confirm everything meets current safety standards. If grounding upgrades are needed, these are usually identified before the SPD is installed.
Once the panel is confirmed suitable, the surge protection device is mounted at or near the main electrical panel and connected according to manufacturer and code requirements. The electrician will then verify that the device is operating correctly, often using a built-in status indicator to confirm protection is active.
Typical installation timeline
For homes with a modern electrical panel and adequate grounding, installation is usually completed within one to two hours. If grounding improvements or minor panel adjustments are required, the work may take longer, but it is still commonly completed in a single visit.
Because the work is done at the main panel, homeowners may experience a brief power interruption during installation. Your electrician should explain what to expect and confirm when power will be restored before beginning work.
Why professional installation matters
Proper installation is essential for surge protection to work as intended. A correctly installed and grounded SPD provides long-term protection with minimal maintenance, while poor installation can reduce effectiveness or leave equipment unprotected. Having both grounding and surge protection addressed together ensures your home’s electrical system is prepared to safely manage voltage surges.
Maintaining Both Protection Systems
Grounding system maintenance
Grounded protection requires very little in terms of regular maintenance. That said, it’s important to conduct periodic checks on your grounding system with a visual inspection of grounding electrode connectors to ensure they’re not damaged or corroded. A professional electrician will also be able to test ground resistance, verifying that there’s a low-resistance pathway for directing voltage and current surges safely to earth.
Surge protection device maintenance
Modern surge protection devices, such as ABB’s, are designed to extremely high safety standards and require very little regular maintenance. Remember that an SPD exists to safeguard your household electrical devices. Depending on the size and frequency of surges, stress on the SPD’s functional parts will gradually degrade its performance and shorten its lifespan.
Many SPDs feature an LED indicator that gives visual confirmation of device status and condition. Depending on the SPD model, an indicator that goes off (or changes colour) warns that the SPD is not providing protection and needs to be replaced. It’s also good practice to replace SPDs after major surge events such as nearby lightning strikes.
When to upgrade your protection
If you haven’t already installed surge protection, it could be time to take action. If you’ve recently added more electronic devices or upgraded smart home systems, adding an SPD can be a wise move that’s repaid by saving delicate tech from costly repairs or replacement. Similarly, if you’re moving to a storm-prone region of the country, whole home surge protection will offer valuable protection for all your household gadgets.
Surge And Grounding Protection: Peace Of Mind For Canadian Homes
Grounded protection is always a minimum prerequisite for home electrical safety, giving vital protection against the dangers of electric shock and household fires. It’s complemented by surge protection that offers a complementary line of defence, safeguarding electronic devices against costly damage caused by sudden voltage spikes.
Modern Canadian homes need both systems working in harmony to keep people and electrical hardware safe. Grounding by itself provides effective shock protection, but it won't safeguard your precious electronic gadgets against damaging power surges.
As today’s homes become smarter and more connected, the integration of proper grounding with whole-home surge protection to protect the myriad of home devices is an increasingly important consideration in every Canadian household.

Frequently Asked Questions
Does grounding provide any surge protection?
Not on its own. Grounding is essential for electrical safety and is a critical part of surge protection systems, but grounding alone does not stop or limit voltage surges. Without a surge protective device (SPD), sudden voltage spikes caused by lightning or utility disturbances can still travel through household wiring and damage connected equipment before excess energy is dissipated to ground.
Can I install surge protection without proper grounding?
No. Surge protection devices depend on a low-resistance grounding path to safely divert excess electrical energy away from household circuits. Without proper grounding, a surge protector cannot function as intended and may fail to protect connected equipment or even create additional safety risks.
Will a whole home surge protector eliminate the need for grounding?
No. Proper grounding is the baseline requirement for household electrical safety and is required regardless of whether surge protection is installed. A whole home surge protector works with the grounding system, not in place of it, to redirect excess voltage safely to earth.
How do I know if my home’s grounding system is adequate for surge protection?
The only reliable way to confirm grounding adequacy is through an inspection by a licensed electrician. They can verify that grounding conductors, bonding connections, and grounding electrodes meet current electrical code requirements and provide a low-impedance path to earth. Older homes, particularly those built before modern grounding standards were adopted, may require upgrades to ensure effective surge protection.
What happens during a power surge if I only have grounding?
If a home relies on grounding alone, a power surge can still travel through branch circuits and connected devices before excess energy is dissipated. This means sensitive electronics may be exposed to damaging overvoltages even though the system is grounded. Grounding helps manage fault currents and provides a discharge path, but without a surge protective device, it does not limit how much voltage reaches household equipment during a surge event.
Important Disclaimer
This article is intended for general informational and educational purposes. Electrical work should be performed by licensed electricians in compliance with local codes and regulations. Consult with qualified professionals for assessment of your specific electrical system needs.