Availability as a functional requirement
Continuous operation brings predictable challenges. Components age. Maintenance work has to be carried out without disrupting the entire process. External conditions introduce variation that cannot be engineered away entirely. In that environment, emissions monitoring is expected to remain online, not because availability is a performance metric in isolation, but because gaps in measurement create uncertainty that compounds quickly.
Moisture, acid gas load and organic components vary significantly in municipal waste streams, making continuous FTIR (Fourier Transform Infrared) measurement a perfect fit for such a complex gas matrix.
FTIR measurement technology is a sophisticated analytical method used in continuous emission monitoring systems to detect and quantify multiple gas pollutants simultaneously. It works by passing infrared light through a gas sample and measuring the unique absorption patterns of different molecules, allowing real-time identification of compounds such as ammonia, hydrogen fluoride, sulfur dioxide and hydrogen chloride in industrial emissions. Unlike traditional single-gas analyzers, FTIR can monitor dozens of gases at once without requiring separate sensors for each pollutant, making it highly efficient for complex emission sources. The technology provides accurate, continuous data that helps industries comply with environmental regulations and optimize combustion processes. The minimal maintenance requirements make FTIR particularly valuable for harsh industrial environments where traditional sensors would fail.
Waste heat recovery, grate temperature control, and flue gas cleaning stages all depend on real-time readings of NOx, SO₂, HCl and CO, which shift quickly as waste composition changes.
At the Nuremberg plant, availability near 95 percent is treated as a working expectation rather than an achievement to be showcased. Monitoring needs to recover quickly after disturbances and continue delivering readable data without requiring extended resets or off line reconciliation.
This is not an abstract concern. It shapes how maintenance is planned, how spares are handled and how much tolerance exists for systems that behave unpredictably under stress.