Success story | April, 2020

ABB has successfully installed Pressductor PillowBlock Load Cells in all Mitsubishi HiTEc Paper Europe's paper and coating machines providing accurate web tension measurement.

 

Mitsubishi HiTec Paper Europe GmbH in Bielefeld – one of the world’s leading manufacturers of special papers – combines the know-how of first-class paper makers with unique technical plant. Sustained by constant product development, consistent market orientation, worldwide sales and state-of-the-art logistics, this is a guarantee of innovation and progress.

As a subsidiary of Mitsubishi Paper Mills of Japan and part of the Mitsubishi Group, Mitsubishi HiTec Paper Bielefeld benefits not only from an excellent international sales network, but also from cooperation on research and development, service and logistics. At the same time the firm has retained the flexibility of a medium-sized enterprise – another advantage for customers.

Mitsubishi HiTec

What we achieved

We asked the Manager for Electrical & Drive Engineering, Mr. Hartmut Schekatz about the load cell installation:

”We have had ABB load cells installed since 1986 and they have been working very well all the time. The ABB load cells work very well in dirty and rough environments and it really doesn’t matter what the environment looks like. Despite rough environments, the load cells always have good and stable signal.”

“We don’t have to adjust the ABB load cells more than once a year.”

“You can have the electronics installed far away, up to 50 meters, from the load cells. This is a very good feature, since the electronics cannot take too much heat created from the paper machines and coaters.”

“We are very satisfied with ABB load cells and electronics and we get a very good support from ABB in Germany. We feel that good business relations are very important.”

“What we appreciate the most is that we don’t have to check the ABB load cells on an every day basis. They are very reliable.”

ABBs solution 

ABB Force Measurement have supplied Mitsubishi HiTec Paper Europe GmbH, Bielefeld, Germany with 32 Pressductor PillowBlock load cells, mostly model PFTL 101A.

Pressductor PillowBlock Load Cells are designed for horizontal or vertical force measurement. Horizontally measuring load cells are ideal in applications with high tare and relatively small tensions, such as paper machines.

 

PBT
Mitsubishi HiTec
Mitsubishi HiTec

Share this page

Discover more

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language